Hello bvilletechwizards,
Based on info found in one of our other posts on how to ID such caps here: SMT Electrolytic Capacitor with no Voltage Rating
looks like the one marked 3h 47 VZA is the 47uF at 35V capacitor such as PCE3842CT-ND you’ll have to check the landing size to make sure, but there are other options also possible here.
That other one marked K1 22C WJ looks like it could be the 22uF at 16V. I’m not too sure on this one though. Something like 1189-1540-1-ND.
There are some other options here.
Hope that helps.