Are there any built-in type reflective Optical Sensors with a sensing distance of a few hundred mm?

Question:

Are there any built-in type reflective Optical Sensors with a long sensing distance of a few hundred millimeters?

Block

Answer:

For long-range detection by a photosensor, consider using the diffuse reflective type Optical Sensor B5W-DB series.

Block

Explanation:

B5W-DB series is the built-in type diffuse reflective type sensor. Even though it is small, its sensing distance is 550 mm (white paper) and long-distance detection is possible. In addition, it is equipped with a circuit that is not easily affected by external light due to its modulated light system. Typical applications include sanitary and disinfecting devices, used as touchless switches to detect palms or hands. For details, see B5W-DB datasheet.


Block

Quick tips

The sensing distance described in the datasheet is specified for a white paper. When designing actual equipment, consider the size, shape, surface condition, and reflectivity of the sensing object, and perform a sufficient evaluation. For applications requiring adjustment of the sensing distance, such as when there is a background object, consider using the B5W-DB11A1. The sensing distance can be varied from 150 to 550 mm (white paper) by the limited resistance value outside the sensor. For details, see B5W-LB11A1: datasheet.


Product category

Sensors Light Convergent Reflective Sensors/Diffuse Reflective Sensors


Classification

Selection, Characteristics


Related keywords

Optical Sensor
Diffuse Reflective Type Sensor
Long-Range Detection
Touchless Switch
Sanitary Equipment
Disinfecting Devices
B5W-DB

Block

Please visit the link below to see this product line on the Digi-Key website
Optical Sensors | Digi-Key Electronics


This FAQ has been brought to you courtesy of




Please click the link below to view the original FAQ

https://components.omron.com/us-en/faq/sensors/FAQE40046