Availability of LRS-100-24?

I recall DigiKey having a significant stock of the Mean Well LRS-100-24 recently. I believe there were 1000+ units available.

It now appears to have been removed from the DigiKey website entirely. Does anyone know if there’s a reason it was removed, or if DigiKey expects to restock it?

I’m specifically wondering whether this is just a temporary inventory issue or if the part has been discontinued/removed from their catalog.

Any information on availability or expected restock would be appreciated. Thanks!

Due to Hunan Aihua Group Co., Ltd. (AiSHi) being added to the UFLPA Entity List, impacted suppliers have been working with our team to identify products affected by the restriction. We have halted sales of select products until further notice. Our customer service and engineering teams are standing by to assist customers in finding a suitable replacement.

Mean Well is one of those impacted suppliers.

If you do not need DC input, one alternative for this would be

PMT-24V100W2BA

Check the datasheet to see if this would work for you.


Thank you very much for the help and insight. This alternative looks great!

For anyone who needs the DC input, our MicroPower Direct MPE-100C-24 is another option: 24 V / 4.5 A (108 W), 85–264 VAC or 120–370 VDC input, in the same 129 x 97 x 30 mm case size. Please check the datasheet for mounting and terminal positions. Datasheet: https://www.digikey.com/en/products/detail/micropower-direct/MPE-100C-24/26228291?s=N4IgTCBcDaILIAUCiBaAjABgwYRWALCALoC%2BQA

Not only LRS, same for other Mean Well parts now. If PSU goes into your product, qualify second source right away and keep it in BOM as alternate. Regulation can stop a part overnight even when stock is 1000+.

After checking the datasheet, the PMR-24V150W1AT is another option, as it also can handle a DC input.