good morining
i need Battery Serial Number: Panasonic LC-P1238AP to fit Cabinet Dimensions: 24" high by 24" wide by 16" deep what battery to do suggest i buy i need 23 of them
good morining
i need Battery Serial Number: Panasonic LC-P1238AP to fit Cabinet Dimensions: 24" high by 24" wide by 16" deep what battery to do suggest i buy i need 23 of them
Hello,
Unfortunately, we do not carry part number LC-P1238AP.
What would a replace be ?
Here is a link to the closest we would have.
12 V Batteries Rechargeable (Secondary) | Electronic Components Distributor DigiKey
Will this one work ?
GS Yuasa battery
Size / Dimension
7.74" L x 6.50" W x 6.89" H (196.6mm x 165.1mm x 175.0mm)
Termination Style
Nut and Bolt, M5
I cannot say for sure but the measurements are real close.
Hi agiammanco,
Dimensionally, it looks like a pretty close match.
Regarding termination, I have not found a datasheet specifically for the LC-P1238AP, but from what I can tell, the “A” in the part number calls out a threaded post of either 5mm or 6mm rather than a square vertical terminal with a 5mm hole which would require a nut and bolt. Unfortunately, because I have not found the documentation for that particular battery, I don’t know whether it’s a 5mm or 6mm threaded post, though most Panasonic batteries seem to use the 5mm posts.
Threaded post:
Nut and Bolt terminal:
It does not appear that we offer any options with either a 5mm or 6mm post, but if you can use the Nut and Bolt option, then the GS Yuasa NP38-12B from our Marketplace would be an option.
If you need a battery that would ship directly from DigiKey and you could use a battery terminal with a female M6 threaded terminal and the accompanying M6 bolt and lock washers, then the EB50-12-I2 or the BP40-12-I2 might be an option.