Wi-Fi 6E is a new band that was added with the introduction of Wi-Fi 6. This allows the use of 6 GHz spectrum.
What are the benefits of Wi-Fi 6E?
- More capacity - The use of 6 GHz allows for up to 1.2 GHz of new spectrum.
Note: Not all countries/regulatory regions use all of the spectrum allowed. Please check the requirements of your specific regions.
- More Channels - With the additional frequencies this allows for more channels:
- Up to 59 20 MHz wide channels.
- Up to 29 40 MHz wide channels.
- Up to 14 80 MHz wide channels.
- Up to 7 160 MHz wide channels.
- No Legacy Devices - The 6 GHz band requires the use of Wi-Fi 6E and OFDMA, so no legacy devices will be able to use the channels. Meaning that there is not any slowdown due to having to support older devices.
- No interference from Microwave Ovens - The 6 GHz band is outside of the frequencies of microwave ovens, so it is not susceptible to interference from them.
What are the drawbacks of Wi-Fi 6E?
- Range - The 6 GHz has a shorter wavelength than 2.4 GHz or 5 GHz, so it will not broadcast as far.
- Interference - With a shorter wavelength, it is not as good at penetrating walls and other obstructions as 2.4 GHz and 5 GHz can.
Source - https://www.lairdconnect.com/support/faqs/what-are-the-benefits-and-drawbacks-of-wi-fi-6e