Board Design Advice Based on My 555 Timer Application

I think it’s a good idea to go over some potential guidelines if you have never made a printed circuit board (PCB) before. I will talk about what I ended up sending for fabrication, but might suggest designing yours a bit different if you do download the files. PCB Routing on an EDA program is a bit different compared to a schematic. Yes, it needs to be a 1:1 electrical equivalent, but the choices are nearly endless for how you lay it out. The goal of my design was to only use a dual sided board with no in-between layers. Extra layers tend to make things more complicated in general. Here are some things I knew beforehand using the Bantam development kit (see this post for reference):

  • Avoid making pads for direct wires if you don’t have headers for test points. Wires are notoriously hard to directly solder to a PCB. Instead, it is often recommended to use surface mount or through hole terminal blocks.
  • Small pads may not make the best connection to small tracks. Professional services like DKRed may not have issues like this anymore, but acid traps may still happen. If you don’t know what this is, extreme angles can literally trap the acid that eats away copper to form traces in the process. This can cause pads to corrode.
  • Small pads are also much harder to solder pins to. Utilize the DigiKey Ruler as a guideline for pad sizes.
  • Use vias when necessary, they make electrical bridges between the top and bottom layer. Unique wires (called nets or traces) cannot overlap in KiCAD. It will stop you from doing so. Vias can be avoided, but use them if you must. They do not typically impact performance.
  • You don’t have to use both sides for your traces. Generally speaking, GND is often made into something called a “pour.” Think of this as one “large wire” that covers all the connection points at once. You don’t have to make it a pour if you don’t want, but it is a good practice.
  • Make sure your footprints are correct. These are physical layouts of where your pins will be placed (either surface mount or through hole). EDA files can be wrong sometimes. Use datasheets or find a drawing that gives you dimension tolerances for layouts and compare. Do your best to find a 3D model for the part or at best a similar 3D model. If you have to, reverse engineer a basic model on a CAD program for a stand in on your board.

As I mentioned in my previous post about the KiCAD schematic, I followed the guidelines in the YouTube playlist as a reference. I made GND my top plane and Vcc as a bottom plane as a pour. Later, I learned that this may not have been ideal or best practice because my ground plane is considered “fragmented.” There technically is electrical connection everywhere, but I am overly segmenting it which could cause noise issue for other circuits. My application is incredibly low frequency, so it’s not a huge concern. Style wise, it is also not very “clean looking.”

More Routing Tips for Beginners

  • Make sure your highest amperage is handled by being sized appropriately with the right trace width. You can use the PCB-RULER-ND as a guide or visit our calculator for trace widths. If you aren’t sure what the highest current is, you can utilize a measurement technique using a shunt resistor, click here to learn more. For my application, I believe a good estimate for the highest possible current would be approximately 105mA (two LEDs, and my timing resistors added up).
  • Did you know you can route under parts? You don’t have to mind the borders around parts (both silkscreen and courtyards). KiCAD will follow rules for tolerance around the existing pads (connection points) and other traces you setup. The pink lines you may see around parts are called courtyards, these are setup so you don’t overlap physical parts.
  • Try to avoid 90 degree turns or 90 degree junctions. This isn’t usually a problem for low frequency design, but are problematic for high frequency.
  • Try to minimize trace lengths. They don’t create much resistance, but traces prevent other traces from being made depending on how many you have! Longer traces also break up the pour you are working on. This could potentially create noise problems too. Here is how I visualize my ground plane:

    These are the regions that I can clearly make out. In essence, I’ve created three “meshes” or “regions” connected by narrower “sub-regions” that act like larger traces. These narrow regions cause impedances to increase and cause higher current density spots. Again, not a big deal for low frequency.
  • Try to find standard footprints for common parts. This includes resistors, capacitors, some potentiometers, DC jacks, headers, etc… You don’t need to create or import footprints for every device you have.
  • Make orientations for polarized parts consistent. Even though electrically it doesn’t matter, assembly is a different question. Even though you might know how it hooks up, mistakes can happen. Someone else who isn’t experienced may not know either. For example, if a polarized capacitor is horizontal to the left, make the other polarized capacitors face the same direction. I did not do this for my design.
  • Select similar sized components for common parts or the same footprints. I chose a different size for R8 with more wattage than I needed. This made it bigger.

    Again, electrically it doesn’t matter, but visually and style wise it does. In the instance where you don’t have access to the same size components, you can make flexible footprints. Potentiometer R5 has a different footprint than R2. Here is what a flexible design would look like:
  • If your power line (typically Vcc or Vdd) doesn’t have many connections, you probably don’t need to make it a pour on one side. Keep them as dedicated traces wide enough to handle the current required.
  • Avoid hiding the references on the silkscreen (light tan color) by the parts. Leave room to keep the references. This helps with assembly if you are going off a BOM.
  • Shapes of components matter too. My red LED for the non-ideal side doesn’t have a flat edge for the negative side. This means you have to double check the datasheet if you are unsure. Installation should be as seamless as possible.
  • To aid soldering your pads, add an offset to allow room for an soldering iron:

Full Design: Files and Pictures

Here are the snapshots of my final design. Keep in mind that I didn’t fix some of the issues I mentioned as this was part of my learning process. This was sent to production.

This is what a KiCAD design looks like with all layers visible (front and back copper, solder masks, and silk screens).

Using ALT + 3, you can load a 3D view of your board! This is what the top looks like without parts populated. This layer excluding the traces is all a GND net.

This is the bottom. This layer is flooded with VCC as a net. There aren’t parts populated.

Here are is the top with the parts populated.

Finally, here is the physical board that I soldered:

Full KiCAD Download

This file includes all 3D files used. Feel free to modify as you please.
final_555_PCB_FullExport.zip (1.2 MB)

Other Documentation

I want you to have access to my pictures and diagrams as well as my in-depth notes, excel data, and datasheets. The files are too big for the TechForum, so they will be Google Drive links:
Documentation
Pictures