Hello, I have an odd shaped board. It’s largest rectangle it fits into is 1.320" x 0.760". However it’s showing up as 0.9997 x 0.5998 on the PCB builder. The preview image looks correct. Is this just the builder incorrectly measuring because of the non rectangular nature of the board or is there something wrong and I won’t receive it as it’s shown in the preview?
Thanks,
-Ben
Thank you for your inquiry.
Dimensions that do not quite match for irregularly shaped boards is something we’ve seen in the past. The board you receive should match what you’re seeing in the preview.
Thanks for the quick reply! Just to make sure though, you say “Dimensions that do not quite match”. It’s not that it says 0.9997" x 0.5998" and should be 1" x 0.6", it’s off by about 20%. Do you still think that’s okay?
Yes. Should be good as long as the preview matches what you expect to be seeing.