Cable M12-12 pin available length

Hey!

do you have cable M12-12 Pin, male-female or male-male?

and what is the longest cable of these types you have?

thank you!

i saw the following SKU, do you have that in Male-Male, and in singular units? 21348485C78200

Hello shira_wisniak,

Welcome to the TechForum and thanks for posting!

I found part number 1754-M12A12ML-12AML-SB002-ND. This is a male to male cable that measures 6.56’.

Thank you!

Just went through the link and saw this it’s only 2 meter long, i need at least 17m,

so if you’ll find anything relevant that will be great.

thanks again!

The closest to that I could find is 1754-M12A12ML-12AML-SB010-ND, but that is a non stocking part and only 10m long. We don’t have any that are the same as 1754-M12A12ML-12AML-SB002-ND and that are 17m long unfortunately.

All other similar options are here: Circular Cable Assemblies | Electronic Components Distributor DigiKey

But those are also not in stock and also at 10m length. We have nothing to offer in 17m long cable with connections of M12 at 12 positions on both ends.

Sorry for the inconvenience.

Hi shira_wisniak,

The only M12 to M12 cable that we normally stock is the following:

Phoenix Contact 1421789 20 meter M12 A-coding Receptacle w/male pins to Plug w/female sockets

Other than this, in 20+ meter lengths, we only have single-ended cables with various M12 connectors on one end and bare wire leads on the opposite end which would require the user to add their own M12 connector.