Cables with intern'l color coding, low smoke, zero halogen

Hi,

We need to redo all of our cables so they meet international color coding standards. (brown, blue, green/yellow, black, etc.) Do you have low smoke zero halogen cables with international color coding?

Thanks,
Chris

Hi fisichel,
Welcome to the DigiKey TechForum. Do you have more information on the cable, do you need single conductor or multiple conductor? What wire gauge do you need? Voltage rating? If you can provide the specifications for the wire it will assist us in finding options for you.

Hi Steve,

Thanks for replying. We have to replace all of our cables. We have multiple conductor cables. 16 AWG (1, 3 and 4 conductors). With braided shielding. The shielding needs to be copper. Not all of of the single conductor cables have shielding.

20 AWG: (1, 2 and 4 conductors) On the single conductor cables, there is not shielding.

22 AWG: (2 and 3 conductors) both of these cables need copper shielding.

The voltage rating is around 1000 VDC.

We still need the international color coding, low smoke and zero halogen characteristics.

Best Regards,
Chris

I found this cable:
Alpha Wire 1178L SL005 Multi-Conductor Cables
It does not have shielding, but it is at least a start.

Best Regards,
Chris

Entering LSZH into a DigiKey search box yields a bunch of hits. That is the magic search term.

Hi Chris,
Sorry for the delay, I was checking for cable with the specifications you listed and I wasn’t able to match all the specs but take a look at this list of multiconductor cables and this list of single conductor cables for options, all are low smoke zero halogen in the wire gauge range and number of conductors you listed. Be sure to check the voltage rating and shield material to verify if these will be sufficient for your application.

Hi Steve,

Those are great finds. We need hook up wire, so that is one less cable to find now. Thanks for sharing those links. I did not see them in my review this morning.

Best Regards,
Chris