Can a relay be mounted in any direction?

Question:

Can a relay be mounted in any direction?

Block

Answer:

Typically the mounting direction is not specified, but some models may have the mounting direction in its specification. Check the datasheet before mounting.

Block

Explanation:

Depending on the operating type and structure of the relay, some relays are easily affected by the mounting direction and others are not.
Normally, the operating characteristics in any mounting direction are within the standard range. However, for models with a large change in operating characteristics depending on the mounting direction, the direction may be specified or conditions may be added.

Refer to G7EB: Correct Use as an example.

Block

Quick tips

Make sure that there is no problem in the actual mounting direction before use.

Block

Please visit the link below to see this product line on the Digi-Key website
Relays | Digi-Key Electronics


This FAQ has been brought to you courtesy of




Please click the link below to view the original FAQ
https://components.omron.com/us-en/faq/relays/FAQE10051