VRWM
The reverse working maximum voltage (VRWM ) is defined as the voltage that can be applied to a TVS diode with an assurance that the diode will not, over process or temperature, conduct significant current.
VBR
The breakdown voltage (VBR ) is the voltage where a TVS diode begins to conduct current, defined typically at 1 mA leakage. VBR defines the inflection point on the diode curve where the leakage beings to increase exponentially, which is typically referred as the diode ‘turning on’.
Please visit the link below to see this product line on the Digi-Key website
Circuit Protection | Transient Voltage Suppressors (TVS) | TVS
This FAQ has been brought to you courtesy of