Hello,
I’m trying to identify this connector :
I need a male & female crimp connector.
Thanks in advance if you can help me.
Hello! Thank you very much for reaching out to us. I hope that what I found is helpful.
After doing some digging, I believe the part number pictured is the TE Connectivity 936119-1. The documentation for it can be found on the TE Connectivity website on the following link:
The datasheet for the 936119-1 specifies the 928999 crimp contacts for 20~24AWG wire and the 963715 contacts for 18~20AWG wire. They are available from the following link:
The cable mounted mate for that connector is the TE Connectivity 936121-1. Additional documentation for that connector is available on the TE Connectivity site on the following link:
The datasheet for the 936121-1 specifies the 928918 contacts for 20~24AWG wire and the 963716 contacts for 18~20AWG wire. They are available from the following link:
I have found, however, that we do stock the 1-936119-1, DigiKey part number A142501-ND, which is the same housing as the 936119-1, but has a white CPA (Connector Position Assurance) device for locking the two connectors together more securely.