CnC Tech is an interconnect supplier offering a useful range of connectors, cables, and similar products. This includes their 2725-2828-BL-01000 cabling, which comes in a variety of value-added lengths from DigiKey but is supplied from the manufacturer with either a -A or a -T suffix. What is the difference between these two suffixes?
In this case, -A and -T refer to the material used for the cable’s braided shielding. -A indicates aluminum alloy braiding, while -T indicates tinned copper braiding. No other specification changes exist between these two suffixes.