Hi Techies,
i need a replacement for the MPN TPS76901SDBVTEP, other than TPS76901QDBVRG4Q1, operating temperature should be -55.
Regards,
Ragav T
Hi Techies,
i need a replacement for the MPN TPS76901SDBVTEP, other than TPS76901QDBVRG4Q1, operating temperature should be -55.
Regards,
Ragav T
Hello @Ragavan.T
You can use the website filters to narrow down the results based on the parameters you need. However, I was unable to find an alternate part that exactly matches TPS76901SDBVTEP
Hi Ragavan.T,
Is there a reason you can’t use the TPS76901SDBVTEP itself? There are currently over 900 pieces in stock and ready to ship?
If the -55°C spec is a hard requirement and you can not use the TPS76901SDBVTEP for some reason, then here’s a link to all of our linear regulators which can operate at -55°C. Some of these are only rated up to 125°C and none of them will exactly match both the electrical and physical characteristics of the TPS76901SDBVTEP.
Knowing your input voltage range and output voltage and current requirements, along with any other special requirements would help to narrow that list down, but the link above would be a starting place. If both physical and electrical requirements must be a near match, then I don’t know of any other part which will meet those specs.