Here is the full boot log:
U-Boot 2018.09-00002-gd5b4c4b656 (Oct 19 2018 - 14:16:02 -0500), Build: jenkins-
github_Bootloader-Builder-84
CPU : AM335X-GP rev 2.1
I2C: ready
DRAM: 512 MiB
No match for driver 'omap_hsmmc'
No match for driver 'omap_hsmmc'
Some drivers were not found
Reset Source: Power-on reset has occurred.
RTC 32KCLK Source: External.
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Loading Environment from EXT4... ** File not found /boot/uboot.env **
** Unable to read "/boot/uboot.env" from mmc0:1 **
Board: BeagleBone Black
<ethaddr> not set. Validating first E-fuse MAC
BeagleBone Black:
Timed out in wait_for_event: status=0000
Check if pads/pull-ups of bus are properly configured
BeagleBone: cape eeprom: i2c_probe: 0x54:
Timed out in wait_for_event: status=0000
Check if pads/pull-ups of bus are properly configured
BeagleBone: cape eeprom: i2c_probe: 0x55:
Timed out in wait_for_event: status=0000
Check if pads/pull-ups of bus are properly configured
BeagleBone: cape eeprom: i2c_probe: 0x56:
Timed out in wait_for_event: status=0000
Check if pads/pull-ups of bus are properly configured
BeagleBone: cape eeprom: i2c_probe: 0x57:
Net: eth0: MII MODE
cpsw, usb_ether
Press SPACE to abort autoboot in 2 seconds
board_name=[A335BNLT] ...
board_rev=[000C] ...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
gpio: pin 56 (gpio 56) value is 0
gpio: pin 55 (gpio 55) value is 0
gpio: pin 54 (gpio 54) value is 0
gpio: pin 53 (gpio 53) value is 1
switch to partitions #0, OK
mmc0 is current device
gpio: pin 54 (gpio 54) value is 1
Checking for: /uEnv.txt ...
Checking for: /boot.scr ...
Checking for: /boot/boot.scr ...
Checking for: /boot/uEnv.txt ...
gpio: pin 55 (gpio 55) value is 1
2128 bytes read in 20 ms (103.5 KiB/s)
Loaded environment from /boot/uEnv.txt
Checking if uname_r is set in /boot/uEnv.txt...
gpio: pin 56 (gpio 56) value is 1
Running uname_boot ...
loading /boot/vmlinuz-5.1.3-bone3 ...
8229376 bytes read in 539 ms (14.6 MiB/s)
debug: [enable_uboot_overlays=1] ...
debug: [enable_uboot_cape_universal=1] ...
debug: [uboot_base_dtb_univ=am335x-boneblack-uboot-univ.dtb] ...
uboot_overlays: [uboot_base_dtb=am335x-boneblack-uboot-univ.dtb] ...
uboot_overlays: Switching too: dtb=am335x-boneblack-uboot-univ.dtb ...
loading /boot/dtbs/5.1.3-bone3/am335x-boneblack-uboot-univ.dtb ...
206146 bytes read in 40 ms (4.9 MiB/s)
uboot_overlays: [fdt_buffer=0x60000] ...
uboot_overlays: loading /lib/firmware/BB-BONE-eMMC1-01-00A0.dtbo ...
1440 bytes read in 52 ms (26.4 KiB/s)
uboot_overlays: uboot loading of [/lib/firmware/BB-HDMI-TDA998x-00A0.dtbo] disab
led by /boot/uEnv.txt [disable_uboot_overlay_video=1]...
uboot_overlays: loading /lib/firmware/BB-ADC-00A0.dtbo ...
711 bytes read in 167 ms (3.9 KiB/s)
uboot_overlays: loading /lib/firmware/AM335X-PRU-RPROC-4-14-TI-00A0.dtbo ...
3513 bytes read in 148 ms (22.5 KiB/s)
uboot_overlays: [dtb_overlay=/lib/firmware/BB-HDMI-CEC-TDA998x-00A0.dtbo] ...
uboot_overlays: loading /lib/firmware/BB-HDMI-CEC-TDA998x-00A0.dtbo ...
5323 bytes read in 77 ms (67.4 KiB/s)
loading /boot/initrd.img-5.1.3-bone3 ...
4895831 bytes read in 330 ms (14.1 MiB/s)
debug: [console=ttyO0,115200n8 bone_capemgr.uboot_capemgr_enabled=1 root=/dev/mm
cblk0p1 ro rootfstype=ext4 rootwait coherent_pool=1M net.ifnames=0] ...
debug: [bootz 0x82000000 0x88080000:4ab457 88000000] ...
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Ramdisk to 8fb54000, end 8ffff457 ... OK
reserving fdt memory region: addr=88000000 size=94000
Loading Device Tree to 8fabd000, end 8fb53fff ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 5.1.3-bone3 (voodoo@w7-imx6q-wandboard-2gb) (gcc ve
rsion 6.3.0 20170516 (Debian 6.3.0-18+deb9u1)) #1stretch PREEMPT Thu May 16 23:2
7:18 UTC 2019
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=50c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instructio
n cache
[ 0.000000] OF: fdt: Machine model: TI AM335x BeagleBone Black
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0x9d000000
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon)
[ 0.000000] random: get_random_bytes called from _etext+0x400935/0x448a52 wit
h crng_init=0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129920
[ 0.000000] Kernel command line: console=ttyO0,115200n8 bone_capemgr.uboot_ca
pemgr_enabled=1 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait coherent_pool=1M
net.ifnames=0
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 449356K/524288K available (8192K kernel code, 984K rwdata
, 3036K rodata, 1024K init, 322K bss, 25780K reserved, 49152K cma-reserved, 0K h
ighmem)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] ftrace: allocating 38908 entries in 76 pages
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jif
fies.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrup
ts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000017] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478
484971ns
[ 0.000042] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max
_idle_ns: 79635851949 ns
[ 0.000053] OMAP clocksource: timer1 at 24000000 Hz
[ 0.001596] timer_probe: no matching timers found
[ 0.001864] Console: colour dummy device 80x30
[ 0.001893] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.001900] This ensures that you still see kernel messages. Please
[ 0.001906] update your kernel commandline.
[ 0.001953] Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)
[ 0.021415] pid_max: default: 32768 minimum: 301
[ 0.021703] LSM: Security Framework initializing
[ 0.021792] Yama: becoming mindful.
[ 0.021847] SELinux: Initializing.
[ 0.021982] *** VALIDATE SELinux ***
[ 0.021997] TOMOYO Linux initialized
[ 0.022070] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.022084] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.022783] *** VALIDATE proc ***
[ 0.023063] *** VALIDATE cgroup1 ***
[ 0.023076] *** VALIDATE cgroup2 ***
[ 0.023134] CPU: Testing write buffer coherency: ok
[ 0.023180] CPU0: Spectre v2: using BPIALL workaround
[ 0.024071] Setting up static identity map for 0x80100000 - 0x80100054
[ 0.024219] rcu: Hierarchical SRCU implementation.
[ 0.026825] EFI services will not be available.
[ 0.028362] devtmpfs: initialized
[ 0.057507] VFP support v0.3: implementor 41 architecture 3 part 30 variant c
rev 3
[ 0.057959] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, ma
x_idle_ns: 7645041785100000 ns
[ 0.057980] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.061679] xor: measuring software checksum speed
[ 0.101395] arm4regs : 1213.000 MB/sec
[ 0.141392] 8regs : 1095.000 MB/sec
[ 0.181394] 32regs : 1093.000 MB/sec
[ 0.221392] neon : 1680.000 MB/sec
[ 0.221400] xor: using function: neon (1680.000 MB/sec)
[ 0.221417] pinctrl core: initialized pinctrl subsystem
[ 0.222145] DMI not present or invalid.
[ 0.222577] NET: Registered protocol family 16
[ 0.226100] DMA: preallocated 1024 KiB pool for atomic coherent allocations
[ 0.301900] l3-aon-clkctrl:0000:0: failed to disable
[ 0.342188] audit: initializing netlink subsys (disabled)
[ 0.343208] cpuidle: using governor menu
[ 0.349463] audit: type=2000 audit(0.340:1): state=initialized audit_enabled=
0 res=1
[ 0.363364] No ATAGs?
[ 0.363374] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.375067] raid6: using algorithm neonx8 gen() 0 MB/s
[ 0.375084] raid6: .... xor() 0 MB/s, rmw enabled
[ 0.375092] raid6: using neon recovery algorithm
[ 0.380782] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.385171] SCSI subsystem initialized
[ 0.385557] usbcore: registered new interface driver usbfs
[ 0.385604] usbcore: registered new interface driver hub
[ 0.385744] usbcore: registered new device driver usb
[ 0.386713] pps_core: LinuxPPS API ver. 1 registered
[ 0.386725] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giome
tti <giometti@linux.it>
[ 0.386746] PTP clock support registered
[ 0.387589] Advanced Linux Sound Architecture Driver Initialized.
[ 0.388187] NetLabel: Initializing
[ 0.388199] NetLabel: domain hash size = 128
[ 0.388205] NetLabel: protocols = UNLABELED CIPSOv4 CALIPSO
[ 0.388282] NetLabel: unlabeled traffic allowed by default
[ 0.389020] clocksource: Switched to clocksource timer1
[ 1.025026] random: fast init done
[ 1.053668] VFS: Disk quotas dquot_6.6.0
[ 1.053744] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 1.064171] NET: Registered protocol family 2
[ 1.065005] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 4096
bytes)
[ 1.065185] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 1.065225] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 1.065263] TCP: Hash tables configured (established 4096 bind 4096)
[ 1.065384] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 1.065402] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 1.065597] NET: Registered protocol family 1
[ 1.066301] RPC: Registered named UNIX socket transport module.
[ 1.066314] RPC: Registered udp transport module.
[ 1.066321] RPC: Registered tcp transport module.
[ 1.066327] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.066637] Unpacking initramfs...
[ 1.350126] Freeing initrd memory: 4784K
[ 1.350729] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counter
s available
[ 1.353388] Initialise system trusted keyrings
[ 1.353678] workingset: timestamp_bits=14 max_order=17 bucket_order=3
[ 1.359743] zbud: loaded
[ 1.362349] NFS: Registering the id_resolver key type
[ 1.362390] Key type id_resolver registered
[ 1.362397] Key type id_legacy registered
[ 1.362414] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 1.362712] fuse init (API version 7.29)
[ 1.608807] Key type asymmetric registered
[ 1.608830] Asymmetric key parser 'x509' registered
[ 1.608929] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 2
46)
[ 1.609347] io scheduler mq-deadline registered
[ 1.613422] OMAP GPIO hardware version 0.1
[ 1.621538] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 100 kHz
[ 1.623459] ti-sysc 48042000.target-module: sysc_flags 00000222 != 00000022
[ 1.624057] ti-sysc 48044000.target-module: sysc_flags 00000222 != 00000022
[ 1.624640] ti-sysc 48046000.target-module: sysc_flags 00000222 != 00000022
[ 1.625351] ti-sysc 48048000.target-module: sysc_flags 00000222 != 00000022
[ 1.625950] ti-sysc 4804a000.target-module: sysc_flags 00000222 != 00000022
[ 1.629221] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 1.631416] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 100 kHz
[ 1.639912] ti-sysc 4830e000.target-module: idlemodes 00000087 != 00000007
[ 1.641246] ti-sysc 4a101200.target-module: rev_offs 00001200 != 00000000
[ 1.641262] ti-sysc 4a101200.target-module: sysc_offs 00001208 != 00000008
[ 1.641272] ti-sysc 4a101200.target-module: syss_offs 00001204 != 00000004
[ 1.669524] pinctrl-single 44e10800.pinmux: 142 pins, size 568
[ 1.679404] gpio-of-helper ocp:cape-universal: ready
[ 1.689332] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 1.691503] Serial: 8250/16550 driver, 6 ports, IRQ sharing disabled
[ 1.694855] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 29, base_baud =
3000000) is a 8250
[ 2.463026] printk: console [ttyS0] enabled
[ 2.468196] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 36, base_baud =
3000000) is a 8250
[ 2.477886] 48024000.serial: ttyS2 at MMIO 0x48024000 (irq = 37, base_baud =
3000000) is a 8250
[ 2.487577] 481a6000.serial: ttyS3 at MMIO 0x481a6000 (irq = 52, base_baud =
3000000) is a 8250
[ 2.497207] 481a8000.serial: ttyS4 at MMIO 0x481a8000 (irq = 53, base_baud =
3000000) is a 8250
[ 2.506756] 481aa000.serial: ttyS5 at MMIO 0x481aa000 (irq = 54, base_baud =
3000000) is a 8250
[ 2.519017] omap_rng 48310000.rng: Random Number Generator ver. 20
[ 3.537039] omap_i2c 4819c000.i2c: timeout waiting for bus ready
[ 4.549028] omap_i2c 4819c000.i2c: timeout waiting for bus ready
[ 5.561030] omap_i2c 4819c000.i2c: timeout waiting for bus ready
[ 6.573027] omap_i2c 4819c000.i2c: timeout waiting for bus ready
[ 7.585029] omap_i2c 4819c000.i2c: timeout waiting for bus ready
[ 8.597027] omap_i2c 4819c000.i2c: timeout waiting for bus ready
[ 9.609029] omap_i2c 4819c000.i2c: timeout waiting for bus ready
[ 10.621027] omap_i2c 4819c000.i2c: timeout waiting for bus ready
[ 10.629219] eqep 48300180.eqep: ver. 1.0
[ 10.633348] eqep 48300180.eqep: count_mode:0
[ 10.637666] eqep 48300180.eqep: invert_qa:1
[ 10.641880] eqep 48300180.eqep: invert_qb:1
[ 10.646094] eqep 48300180.eqep: invert_qi:0
[ 10.650308] eqep 48300180.eqep: invert_qs:0
[ 10.654522] eqep 48300180.eqep: swap_inputs:0
[ 10.658910] eqep 48300180.eqep: QDECCTL:0x0180
[ 10.663384] eqep 48300180.eqep: QPOSINIT:0x00000000
[ 10.668293] eqep 48300180.eqep: QPOSMAX:0xffffffff
[ 10.673117] eqep 48300180.eqep: QPOSCNT:0x00000000
[ 10.677941] eqep 48300180.eqep: omit_interrupt:0
[ 10.682589] eqep 48300180.eqep: QEINT:0x0800
[ 10.686888] eqep 48300180.eqep: QUPRD:0x05f5e100
[ 10.691534] eqep 48300180.eqep: QEPCTL:0x009e write
[ 10.696445] eqep 48300180.eqep: QEPCTL:0x009e read
[ 10.701281] eqep 48300180.eqep: irq:136, clk_rate:100000000
[ 10.707125] eqep 48302180.eqep: ver. 1.0
[ 10.711182] eqep 48302180.eqep: count_mode:0
[ 10.715494] eqep 48302180.eqep: invert_qa:1
[ 10.719711] eqep 48302180.eqep: invert_qb:1
[ 10.723925] eqep 48302180.eqep: invert_qi:0
[ 10.728138] eqep 48302180.eqep: invert_qs:0
[ 10.732350] eqep 48302180.eqep: swap_inputs:0
[ 10.736736] eqep 48302180.eqep: QDECCTL:0x0180
[ 10.741211] eqep 48302180.eqep: QPOSINIT:0x00000000
[ 10.746120] eqep 48302180.eqep: QPOSMAX:0xffffffff
[ 10.750945] eqep 48302180.eqep: QPOSCNT:0x00000000
[ 10.755768] eqep 48302180.eqep: omit_interrupt:0
[ 10.760415] eqep 48302180.eqep: QEINT:0x0800
[ 10.764713] eqep 48302180.eqep: QUPRD:0x05f5e100
[ 10.769362] eqep 48302180.eqep: QEPCTL:0x009e write
[ 10.774271] eqep 48302180.eqep: QEPCTL:0x009e read
[ 10.779105] eqep 48302180.eqep: irq:138, clk_rate:100000000
[ 10.784899] eqep 48304180.eqep: ver. 1.0
[ 10.788937] eqep 48304180.eqep: count_mode:0
[ 10.793250] eqep 48304180.eqep: invert_qa:1
[ 10.797464] eqep 48304180.eqep: invert_qb:1
[ 10.801678] eqep 48304180.eqep: invert_qi:0
[ 10.805892] eqep 48304180.eqep: invert_qs:0
[ 10.810105] eqep 48304180.eqep: swap_inputs:0
[ 10.814491] eqep 48304180.eqep: QDECCTL:0x0180
[ 10.818965] eqep 48304180.eqep: QPOSINIT:0x00000000
[ 10.823874] eqep 48304180.eqep: QPOSMAX:0xffffffff
[ 10.828696] eqep 48304180.eqep: QPOSCNT:0x00000000
[ 10.833520] eqep 48304180.eqep: omit_interrupt:0
[ 10.838167] eqep 48304180.eqep: QEINT:0x0800
[ 10.842466] eqep 48304180.eqep: QUPRD:0x05f5e100
[ 10.847113] eqep 48304180.eqep: QEPCTL:0x009e write
[ 10.852021] eqep 48304180.eqep: QEPCTL:0x009e read
[ 10.856854] eqep 48304180.eqep: irq:140, clk_rate:100000000
[ 10.898340] libphy: Fixed MDIO Bus: probed
[ 10.903349] CAN device driver interface
[ 10.908805] c_can_platform 481cc000.can: c_can_platform device registered (re
gs=(ptrval), irq=57)
[ 10.918698] c_can_platform 481d0000.can: c_can_platform device registered (re
gs=(ptrval), irq=58)
[ 10.981112] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1
000000
[ 10.988848] libphy: 4a101000.mdio: probed
[ 11.000672] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driv
er SMSC LAN8710/LAN8720
[ 11.010153] cpsw 4a100000.ethernet: Detected MACID = fc:69:47:3a:98:ed
[ 11.016973] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 11.023413] cpsw 4a100000.ethernet: ALE Table size 1024
[ 11.028718] cpsw 4a100000.ethernet: cpts: overflow check period 1250 (jiffies
)
[ 11.038275] usbcore: registered new interface driver usb-storage
[ 11.047595] am335x-phy-driver 47401300.usb-phy: 47401300.usb-phy supply vcc n
ot found, using dummy regulator
[ 11.063642] am335x-phy-driver 47401b00.usb-phy: 47401b00.usb-phy supply vcc n
ot found, using dummy regulator
[ 11.088582] omap_rtc 44e3e000.rtc: registered as rtc0
[ 11.094788] i2c /dev entries driver
[ 11.102161] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 11.109559] softdog: initialized. soft_noboot=0 soft_margin=60 sec soft_panic
=0 (nowayout=0)
[ 11.122027] omap_gpio 44e07000.gpio: Could not set line 6 debounce to 200000
microseconds (-22)
[ 11.130834] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 11.191297] ledtrig-cpu: registered to indicate activity on CPUs
[ 11.197922] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 11.203992] omap-aes 53500000.aes: will run requests pump with realtime prior
ity
[ 11.250310] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 11.304887] mmc1: new high speed MMC card at address 0001
[ 11.315688] mmcblk1: mmc1:0001 DG4008 7.28 GiB
[ 11.325834] mmcblk1boot0: mmc1:0001 DG4008 partition 1 4.00 MiB
[ 11.336742] hidraw: raw HID events driver (C) Jiri Kosina
[ 11.342958] mmcblk1boot1: mmc1:0001 DG4008 partition 2 4.00 MiB
[ 11.349362] usbcore: registered new interface driver usbhid
[ 11.355267] mmcblk1rpmb: mmc1:0001 DG4008 partition 3 4.00 MiB, chardev (244:
0)
[ 11.362666] usbhid: USB HID core driver
[ 11.367666] remoteproc remoteproc0: wkup_m3 is available
[ 11.380449] gnss: GNSS driver registered with major 242
[ 11.388952] NET: Registered protocol family 10
[ 11.437633] Segment Routing with IPv6
[ 11.441561] mip6: Mobile IPv6
[ 11.444550] NET: Registered protocol family 17
[ 11.449130] can: controller area network core (rev 20170425 abi 9)
[ 11.455485] NET: Registered protocol family 29
[ 11.460103] Key type dns_resolver registered
[ 11.464417] mpls_gso: MPLS GSO support
[ 11.468413] ThumbEE CPU extension supported.
[ 11.472730] Registering SWP/SWPB emulation handler
[ 11.477560] omap_voltage_late_init: Voltage driver support not added
[ 11.485763] registered taskstats version 1
[ 11.489929] Loading compiled-in X.509 certificates
[ 11.494864] zswap: loaded using pool lzo/zbud
[ 11.502008] Btrfs loaded, crc32c=crc32c-generic
[ 11.663466] tda998x 0-0070: found TDA19988
[ 11.670965] tilcdc 4830e000.lcdc: bound 0-0070 (ops 0xc097cd84)
[ 11.676998] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 11.683658] [drm] No driver support for vblank timestamp query.
[ 11.690342] [drm] Initialized tilcdc 1.0.0 20121205 for 4830e000.lcdc on mino
r 0
[ 11.698102] [drm] Cannot find any crtc or sizes
[ 11.703611] [drm] Cannot find any crtc or sizes
[ 11.718303] tps6521x_pwrbutton tps65217-pwrbutton: DMA mask not set
[ 11.725282] input: tps65217_pwr_but as /devices/platform/ocp/44c00000.interco
nnect/44c00000.interconnect:segment@200000/44e0b000.target-module/44e0b000.i2c/i
2c-0/0-0024/tps65217-pwrbutton/input/input0
[ 11.743687] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[ 11.749765] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 11.756787] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 11.763593] remoteproc remoteproc0: powering up wkup_m3
[ 11.768959] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf,
size 217168
[ 11.781319] remoteproc remoteproc0: remote processor wkup_m3 is now up
[ 11.781337] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x193
[ 11.796990] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 11.802386] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus numbe
r 1
[ 11.810155] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bc
dDevice= 5.01
[ 11.818525] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=
1
[ 11.825819] usb usb1: Product: MUSB HDRC host driver
[ 11.830867] usb usb1: Manufacturer: Linux 5.1.3-bone3 musb-hcd
[ 11.836757] usb usb1: SerialNumber: musb-hdrc.1
[ 11.842034] hub 1-0:1.0: USB hub found
[ 11.845902] hub 1-0:1.0: 1 port detected
[ 11.855625] omap_rtc 44e3e000.rtc: setting system clock to 2000-01-01T00:00:0
1 UTC (946684801)
[ 11.866262] ALSA device list:
[ 11.869381] No soundcards found.
[ 11.878117] Freeing unused kernel memory: 1024K
[ 11.885492] Run /init as init process
Loading, please wait...
starting version 232
[ 12.335051] random: systemd-udevd: uninitialized urandom read (16 bytes read)
[ 12.350138] random: systemd-udevd: uninitialized urandom read (16 bytes read)
[ 12.363718] random: udevadm: uninitialized urandom read (16 bytes read)
[ 12.459766] musb-hdrc musb-hdrc.1: VBUS_ERROR in a_wait_vrise (80, <SessEnd),
retry #3, port1 0008010c
Begin: Loading essential drivers ... done.
Begin: Running /scripts/init-premount ... done.
Begin: Mounting root file system ... Begin: Running /scripts/local-top ... done.
Begin: Running /scripts/local-premount ... Scanning for Btrfs filesystems
done.
Begin: Waiting for root file system ... Begin: Running /scripts/local-block ...
done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
Begin: Running /scripts/local-block ... done.
done.
Gave up waiting for root file system device. Common problems:
- Boot args (cat /proc/cmdline)
- Check rootdelay= (did the system wait long enough?)
- Missing modules (cat /proc/modules; ls /dev)
ALERT! /dev/mmcblk0p1 does not exist. Dropping to a shell!
BusyBox v1.22.1 (Debian 1:1.22.0-19+b3) built-in shell (ash)
Enter 'help' for a list of built-in commands.
(initramfs)
It seems like after kernel is loaded, it can’t find rootfs partition.
What can cause this?
Thanks