Hello, I’m trying to make my own board based on BBB.
But struggling to make own kernel for my board.
- It is fully working with the 4.19.232-bone-rt-r75 kernel with this am335x-boneblack-uboot-univ.dts and uENV.txt
am335x-boneblack-uboot-univ.dts (190.5 KB)
Here is the successfull u-boot log…
U-Boot 2019.04-dirty (May 04 2023 - 16:45:19 +0900)
CPU : AM335X-GP rev 2.1
I2C: ready
DRAM: 512 MiB
No match for driver 'omap_hsmmc'
No match for driver 'omap_hsmmc'
Some drivers were not found
Reset Source: Power-on reset has occurred.
RTC 32KCLK Source: External.
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Loading Environment from EXT4... ** File not found /boot/uboot.env **
** Unable to read "/boot/uboot.env" from mmc0:1 **
Board: BeagleBone Black
<ethaddr> not set. Validating first E-fuse MAC
BeagleBone Black:
BeagleBone Cape EEPROM: no EEPROM at address: 0x54
BeagleBone Cape EEPROM: no EEPROM at address: 0x55
BeagleBone Cape EEPROM: no EEPROM at address: 0x56
BeagleBone Cape EEPROM: no EEPROM at address: 0x57
Net: eth0: MII MODE
Could not get PHY for cpsw: addr 0
cpsw, usb_ether
Press SPACE to abort autoboot in 0 seconds
board_name=[A335BNLT] ...
board_rev=[] ...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
gpio: pin 56 (gpio 56) value is 0
gpio: pin 55 (gpio 55) value is 0
gpio: pin 54 (gpio 54) value is 0
gpio: pin 53 (gpio 53) value is 1
switch to partitions #0, OK
mmc0 is current device
gpio: pin 54 (gpio 54) value is 1
Checking for: /uEnv.txt ...
Checking for: /boot.scr ...
Checking for: /boot/boot.scr ...
Checking for: /boot/uEnv.txt ...
gpio: pin 55 (gpio 55) value is 1
2527 bytes read in 27 ms (90.8 KiB/s)
Loaded environment from /boot/uEnv.txt
debug: [dtb=am335x-boneblack-emmc-overlay.dtb] ...
Using: dtb=am335x-boneblack-emmc-overlay.dtb ...
Checking if uname_r is set in /boot/uEnv.txt...
gpio: pin 56 (gpio 56) value is 1
Running uname_boot ...
loading /boot/vmlinuz-4.19.232-bone-rt-r75 ...
8491520 bytes read in 565 ms (14.3 MiB/s)
debug: [enable_uboot_overlays=1] ...
debug: [enable_uboot_cape_universal=1] ...
debug: [uboot_base_dtb_univ=am335x-boneblack-uboot-univ.dtb] ...
uboot_overlays: [uboot_base_dtb=am335x-boneblack-uboot-univ.dtb] ...
uboot_overlays: Switching too: dtb=am335x-boneblack-uboot-univ.dtb ...
loading /boot/dtbs/4.19.232-bone-rt-r75/am335x-boneblack-uboot-univ.dtb ...
158926 bytes read in 64 ms (2.4 MiB/s)
uboot_overlays: [fdt_buffer=0x60000] ...
uboot_overlays: uboot loading of [BB-ADC-00A0.dtbo] disabled by /boot/uEnv.txt [disable_uboot_overlay_adc=1]...
uboot_overlays: loading /lib/firmware/BB-UART1-00A0.dtbo ...
1053 bytes read in 370 ms (2 KiB/s)
uboot_overlays: loading /lib/firmware/BB-UART2-00A0.dtbo ...
1053 bytes read in 68 ms (14.6 KiB/s)
uboot_overlays: loading /lib/firmware/BB-UART4-00A0.dtbo ...
1053 bytes read in 216 ms (3.9 KiB/s)
uboot_overlays: loading /lib/firmware/BB-UART5-00A0.dtbo ...
1053 bytes read in 315 ms (2.9 KiB/s)
uboot_overlays: loading /lib/firmware/BB-I2C1-00A0.dtbo ...
1130 bytes read in 358 ms (2.9 KiB/s)
uboot_overlays: loading /boot/dtbs/4.19.232-bone-rt-r75/overlays/BB-BONE-eMMC1-01-00A0.dtbo ...
1605 bytes read in 116 ms (12.7 KiB/s)
uboot_overlays: uboot loading of [BB-HDMI-TDA998x-00A0.dtbo] disabled by /boot/uEnv.txt [disable_uboot_overlay_video=1]...
uboot_overlays: loading /lib/firmware/AM335X-PRU-RPROC-4-19-TI-00A0.dtbo ...
3653 bytes read in 358 ms (9.8 KiB/s)
debug: [console=ttyO0,115200n8 bone_capemgr.uboot_capemgr_enabled=1 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait coherent_pool=1M net.ifnames=0 lpj=1990656 rng_core.default_quality=100 quiet] ...
debug: [bootz 0x82000000 - 88000000] ...
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ff75000, end 8fffffff ... OK
Starting kernel ...
[ 0.001453] timer_probe: no matching timers found
[ 0.268681] l4_wkup_cm:clk:0010:0: failed to disable
[ 0.751026] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 1.205456] omap_voltage_late_init: Voltage driver support not added
[ 15.502381] libphy: PHY 4a101000.mdio:00 not found
[ 15.519376] net eth0: phy "4a101000.mdio:00" not found on slave 0, err -19
Here is the uENV.txt also working well
#uname_r=5.10.168-ti-r63
uname_r=4.19.232-bone-rt-r75
dtb=am335x-boneblack-emmc-overlay.dtb
###U-Boot Overlays###
###Documentation: http://elinux.org/Beagleboard:BeagleBoneBlack_Debian#U-Boot_Overlays
###Master Enable
enable_uboot_overlays=1
uboot_overlay_addr0=/lib/firmware/BB-UART1-00A0.dtbo
uboot_overlay_addr1=/lib/firmware/BB-UART2-00A0.dtbo
uboot_overlay_addr2=/lib/firmware/BB-UART4-00A0.dtbo
uboot_overlay_addr3=/lib/firmware/BB-UART5-00A0.dtbo
uboot_overlay_addr4=/lib/firmware/BB-I2C1-00A0.dtbo
###
###Overide capes with eeprom
#uboot_overlay_addr0=/lib/firmware/<file0>.dtbo
#uboot_overlay_addr1=/lib/firmware/<file1>.dtbo
#uboot_overlay_addr2=/lib/firmware/<file2>.dtbo
#uboot_overlay_addr3=/lib/firmware/<file3>.dtbo
###
###Additional custom capes
#uboot_overlay_addr4=/lib/firmware/<file4>.dtbo
#uboot_overlay_addr5=/lib/firmware/<file5>.dtbo
#uboot_overlay_addr6=/lib/firmware/<file6>.dtbo
#uboot_overlay_addr7=/lib/firmware/<file7>.dtbo
###
###Custom Cape
#dtb_overlay=/lib/firmware/<file8>.dtbo
###
###Disable auto loading of virtual capes (emmc/video/wireless/adc)
#disable_uboot_overlay_emmc=1
disable_uboot_overlay_video=1
disable_uboot_overlay_audio=1
disable_uboot_overlay_wireless=1
disable_uboot_overlay_adc=1
###
###PRUSS OPTIONS
###pru_rproc (4.14.x-ti kernel)
#uboot_overlay_pru=/lib/firmware/AM335X-PRU-RPROC-4-14-TI-00A0.dtbo
###pru_rproc (4.19.x-ti kernel)
uboot_overlay_pru=/lib/firmware/AM335X-PRU-RPROC-4-19-TI-00A0.dtbo
###pru_uio (4.14.x-ti, 4.19.x-ti & mainline/bone kernel)
#uboot_overlay_pru=/lib/firmware/AM335X-PRU-UIO-00A0.dtbo
###
###Cape Universal Enable
enable_uboot_cape_universal=1
###
###Debug: disable uboot autoload of Cape
#disable_uboot_overlay_addr0=1
#disable_uboot_overlay_addr1=1
#disable_uboot_overlay_addr2=1
#disable_uboot_overlay_addr3=1
###
###U-Boot fdt tweaks... (60000 = 384KB)
#uboot_fdt_buffer=0x60000
###U-Boot Overlays###
cmdline=coherent_pool=1M net.ifnames=0 lpj=1990656 rng_core.default_quality=100 quiet
#In the event of edid real failures, uncomment this next line:
#cmdline=coherent_pool=1M net.ifnames=0 lpj=1990656 rng_core.default_quality=100 quiet video=HDMI-A-1:1024x768@60e
##enable Generic eMMC Flasher:
##make sure, these tools are installed: dosfstools rsync
#cmdline=init=/opt/scripts/tools/eMMC/init-eMMC-flasher-v3.sh
cape_disable=bone_capemgr.disable_partno=BB-BONELT-HDMI,BB-BONELT-HDMIN
cape_enable=bone_capemgr.enable_partno=BB-UART1,BB-UART2,BB-UART4,BB-UART5
#optargs=capemgr.enable_partno=BB-UART1,BB-UART2,BB-UART4,BB-UART5
Then, I tried to upgrade it to 5.10.y rt kernel with up to date Debian (I failed to used Debian 12.x. So I ended up to chosen 11.x)
1. I followed the instructions at Debian: Getting Started with the BeagleBone Black
2. I chosed this kernel : am33x-rt-v5.10 (Longterm 5.10.x + Real-Time Linux)
3. I chosed to use debian-11.5-minimal-armhf-2022-10-06
4. After the u-boot I found that there were some failures and couldn’t use the previous gpio configuration successfully worked in the past
U-Boot SPL 2022.04-00037-ge0d31da5-dirty (Nov 01 2023 - 08:35:30 +0900)
Trying to boot from MMC1
U-Boot 2022.04-00037-ge0d31da5-dirty (Nov 01 2023 - 08:35:30 +0900)
CPU : AM335X-GP rev 2.1
Model: TI AM335x BeagleBone Black
DRAM: 512 MiB
Reset Source: Power-on reset has occurred.
RTC 32KCLK Source: External.
Core: 150 devices, 14 uclasses, devicetree: separate
WDT: Started wdt@44e35000 with servicing (60s timeout)
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Loading Environment from EXT4... ** File not found /boot/uboot.env **
** Unable to read "/boot/uboot.env" from mmc0:1 **
Board: BeagleBone Black
<ethaddr> not set. Validating first E-fuse MAC
BeagleBone Black:
BeagleBone Cape EEPROM: no EEPROM at address: 0x54
BeagleBone Cape EEPROM: no EEPROM at address: 0x55
BeagleBone Cape EEPROM: no EEPROM at address: 0x56
BeagleBone Cape EEPROM: no EEPROM at address: 0x57
Net: Could not get PHY for ethernet@4a100000: addr 0
eth2: ethernet@4a100000, eth3: usb_ether
Press SPACE to abort autoboot in 0 seconds
board_name=[A335BNLT] ...
board_rev=[unknown] ...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
Couldn't find partition 0:2 0x82000000
Can't set block device
Couldn't find partition 0:2 0x82000000
Can't set block device
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
Scanning disk mmc@48060000.blk...
Scanning disk mmc@481d8000.blk...
Found 7 disks
No EFI system partition
WARNING: could not set serial-number FDT_ERR_BADVERSION.
ERROR: root node setup failed
- must RESET the board to recover.
ERROR: failed to process device tree
gpio: pin 56 (gpio 56) value is 0
gpio: pin 55 (gpio 55) value is 0
gpio: pin 54 (gpio 54) value is 0
gpio: pin 53 (gpio 53) value is 1
switch to partitions #0, OK
mmc0 is current device
gpio: pin 54 (gpio 54) value is 1
Checking for: /uEnv.txt ...
Checking for: /boot/uEnv.txt ...
gpio: pin 55 (gpio 55) value is 1
735 bytes read in 4 ms (178.7 KiB/s)
Loaded environment from /boot/uEnv.txt
Checking if uname_r is set in /boot/uEnv.txt...
gpio: pin 56 (gpio 56) value is 1
Running uname_boot ...
loading /boot/vmlinuz-5.10.186-bone-rt-r76 ...
9880064 bytes read in 624 ms (15.1 MiB/s)
debug: [enable_uboot_overlays=1] ...
debug: [enable_uboot_cape_universal=1] ...
debug: [uboot_base_dtb_univ=am335x-boneblack-uboot-univ.dtb] ...
uboot_overlays: [uboot_base_dtb=am335x-boneblack-uboot-univ.dtb] ...
uboot_overlays: Switching too: dtb=am335x-boneblack-uboot-univ.dtb ...
loading /boot/dtbs/5.10.186-bone-rt-r76/am335x-boneblack-uboot-univ.dtb ...
199395 bytes read in 17 ms (11.2 MiB/s)
Found 0 extension board(s).
uboot_overlays: [fdt_buffer=0x60000] ...
uboot_overlays: uboot loading of [BB-ADC-00A0.dtbo] disabled by /boot/uEnv.txt [disable_uboot_overlay_adc=1]...
uboot_overlays: loading /boot/dtbs/5.10.186-bone-rt-r76/overlays/BB-UART1-00A0.dtbo ...
1017 bytes read in 6 ms (165 KiB/s)
uboot_overlays: loading /boot/dtbs/5.10.186-bone-rt-r76/overlays/BB-UART2-00A0.dtbo ...
1017 bytes read in 6 ms (165 KiB/s)
uboot_overlays: loading /boot/dtbs/5.10.186-bone-rt-r76/overlays/BB-UART4-00A0.dtbo ...
1017 bytes read in 6 ms (165 KiB/s)
uboot_overlays: loading /boot/dtbs/5.10.186-bone-rt-r76/overlays/BB-I2C1-RTC-PCF8563.dtbo ...
1480 bytes read in 7 ms (206.1 KiB/s)
uboot_overlays: loading /boot/dtbs/5.10.186-bone-rt-r76/overlays/BB-BONE-eMMC1-01-00A0.dtbo ...
1605 bytes read in 7 ms (223.6 KiB/s)
uboot_overlays: uboot loading of [BB-HDMI-TDA998x-00A0.dtbo] disabled by /boot/uEnv.txt [disable_uboot_overlay_video=1]...
debug: [console=ttyS0,115200n8 bone_capemgr.uboot_capemgr_enabled=1 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait coherent_pool=1M net.ifnames=0 lpj=1990656 rng_core.default_quality=100 quiet] ...
debug: [bootz 0x82000000 - 88000000] ...
Kernel image @ 0x82000000 [ 0x000000 - 0x96c200 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ff6b000, end 8fffffff ... OK
Starting kernel ...
[ 1.408534] l3-aon-clkctrl:0000:0: failed to disable
[ 1.438231] omap_voltage_late_init: Voltage driver support not added
[ 1.438516] PM: Cannot get wkup_m3_ipc handle
[ 1.512329] wkup_m3_rproc 44d00000.cpu: Platform data missing!
[ 1.581318] gpiochip_add_data_with_key: GPIOs 0..31 (gpio-0-31) failed to register, -517
[ 1.856338] wkup_m3_ipc 44e11324.wkup_m3_ipc: IPC Request for A8->M3 Channel failed! -517
[ 2.784073] mdio_bus 4a101000.mdio: MDIO device at address 0 is missing.
[ 2.806562] debugfs: Directory '49000000.dma' with parent 'dmaengine' already present!
[ 3.019173] gpio-of-helper ocp:cape-universal: Failed to get gpio property of 'P8_13'
[ 3.019181] gpio-of-helper ocp:cape-universal: Failed to create gpio entry
[ 3.023489] PM: Cannot get wkup_m3_ipc handle
[ 3.117324] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 3.173389] PM: Cannot get wkup_m3_ipc handle
[ 3.174234] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 3.179819] PM: Cannot get wkup_m3_ipc handle
[ 3.180299] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 3.284541] PM: Cannot get wkup_m3_ipc handle
[ 3.285147] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 3.312404] PM: Cannot get wkup_m3_ipc handle
[ 3.312974] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 3.512217] PM: Cannot get wkup_m3_ipc handle
[ 3.512800] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 4.322595] PM: Cannot get wkup_m3_ipc handle
[ 4.323188] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 4.510565] PM: Cannot get wkup_m3_ipc handle
[ 4.511162] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 4.690729] PM: Cannot get wkup_m3_ipc handle
[ 4.691313] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 19.044588] PM: Cannot get wkup_m3_ipc handle
[ 19.045219] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 19.067381] PM: Cannot get wkup_m3_ipc handle
[ 19.068157] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 19.080392] PM: Cannot get wkup_m3_ipc handle
[ 19.081017] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 19.097171] PM: Cannot get wkup_m3_ipc handle
[ 19.098011] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 19.604688] PM: Cannot get wkup_m3_ipc handle
[ 19.605311] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 19.874090] PM: Cannot get wkup_m3_ipc handle
[ 19.874708] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 20.148413] PM: Cannot get wkup_m3_ipc handle
[ 20.149051] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 20.612775] PM: Cannot get wkup_m3_ipc handle
[ 20.613388] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 22.133390] PM: Cannot get wkup_m3_ipc handle
[ 22.133986] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 22.161546] PM: Cannot get wkup_m3_ipc handle
[ 22.162137] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 22.189431] PM: Cannot get wkup_m3_ipc handle
[ 22.190015] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
Here is the dmesg log…
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 5.10.186-bone-rt-r76 (root@yk-VirtualBox) (arm-linux-gnueabi-gcc (GCC) 10.4.0, GNU ld (GNU Binutils) 2.39) #1 SMP PREEMPT Wed Nov 1 11:23:09 KST 2023
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=50c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM335x BeagleBone Black
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0x9c800000
[ 0.000000] Zone ranges:
[ 0.000000] Normal [mem 0x0000000080000000-0x000000009fefffff]
[ 0.000000] HighMem empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009fefffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x000000009fefffff]
[ 0.000000] On node 0 totalpages: 130816
[ 0.000000] Normal zone: 1150 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 130816 pages, LIFO batch:31
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon)
[ 0.000000] percpu: Embedded 17 pages/cpu s37900 r8192 d23540 u69632
[ 0.000000] pcpu-alloc: s37900 r8192 d23540 u69632 alloc=17*4096
[ 0.000000] pcpu-alloc: [0] 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129666
[ 0.000000] Kernel command line: console=ttyS0,115200n8 bone_capemgr.uboot_capemgr_enabled=1 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait coherent_pool=1M net.ifnames=0 lpj=1990656 rng_core.default_quality=100 quiet
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 451024K/523264K available (10240K kernel code, 1572K rwdata, 3440K rodata, 1024K init, 359K bss, 23088K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] ftrace: allocating 43734 entries in 129 pages
[ 0.000000] ftrace: allocated 129 pages with 2 groups
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Rude variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrupts
[ 0.000000] TI gptimer clocksource: always-on /ocp/interconnect@44c00000/segment@200000/target-module@31000
[ 0.000001] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000022] clocksource: dmtimer: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000392] TI gptimer clockevent: 24000000 Hz at /ocp/interconnect@48000000/segment@0/target-module@40000
[ 0.002328] Console: colour dummy device 80x30
[ 0.002393] Calibrating delay loop (skipped) preset value.. 995.32 BogoMIPS (lpj=1990656)
[ 0.002414] pid_max: default: 32768 minimum: 301
[ 0.002990] LSM: Security Framework initializing
[ 0.003099] Yama: becoming mindful.
[ 0.003324] AppArmor: AppArmor initialized
[ 0.003338] TOMOYO Linux initialized
[ 0.003522] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[ 0.003538] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes, linear)
[ 0.005147] CPU: Testing write buffer coherency: ok
[ 0.005212] CPU0: Spectre v2: using BPIALL workaround
[ 0.007142] Setting up static identity map for 0x80100000 - 0x80100054
[ 0.007380] rcu: Hierarchical SRCU implementation.
[ 0.008774] EFI services will not be available.
[ 0.009088] smp: Bringing up secondary CPUs ...
[ 0.009097] smp: Brought up 1 node, 1 CPU
[ 0.009106] SMP: Total of 1 processors activated (995.32 BogoMIPS).
[ 0.009117] CPU: All CPU(s) started in SVC mode.
[ 0.009892] devtmpfs: initialized
[ 0.049967] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.050444] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.050475] futex hash table entries: 256 (order: 2, 16384 bytes, linear)
[ 0.054291] pinctrl core: initialized pinctrl subsystem
[ 0.056322] NET: Registered protocol family 16
[ 0.061179] DMA: preallocated 1024 KiB pool for atomic coherent allocations
[ 0.061767] audit: initializing netlink subsys (disabled)
[ 0.062994] thermal_sys: Registered thermal governor 'fair_share'
[ 0.063007] thermal_sys: Registered thermal governor 'bang_bang'
[ 0.063011] thermal_sys: Registered thermal governor 'step_wise'
[ 0.063925] cpuidle: using governor menu
[ 0.068539] audit: type=2000 audit(0.060:1): state=initialized audit_enabled=0 res=1
[ 0.140180] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.166279] raid6: skip pq benchmark and using algorithm neonx8
[ 0.166299] raid6: using neon recovery algorithm
[ 0.167917] iommu: Default domain type: Translated
[ 0.171331] SCSI subsystem initialized
[ 0.171404] libata version 3.00 loaded.
[ 0.171727] usbcore: registered new interface driver usbfs
[ 0.171783] usbcore: registered new interface driver hub
[ 0.171840] usbcore: registered new device driver usb
[ 0.172292] pps_core: LinuxPPS API ver. 1 registered
[ 0.172301] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.172323] PTP clock support registered
[ 0.174492] NetLabel: Initializing
[ 0.174505] NetLabel: domain hash size = 128
[ 0.174511] NetLabel: protocols = UNLABELED CIPSOv4 CALIPSO
[ 0.174591] NetLabel: unlabeled traffic allowed by default
[ 0.175708] clocksource: Switched to clocksource dmtimer
[ 1.272499] VFS: Disk quotas dquot_6.6.0
[ 1.272620] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 1.273751] AppArmor: AppArmor Filesystem Enabled
[ 1.286258] NET: Registered protocol family 2
[ 1.286511] IP idents hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 1.287996] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear)
[ 1.288103] TCP established hash table entries: 4096 (order: 2, 16384 bytes, linear)
[ 1.288148] TCP bind hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 1.288207] TCP: Hash tables configured (established 4096 bind 4096)
[ 1.288329] UDP hash table entries: 256 (order: 1, 8192 bytes, linear)
[ 1.288355] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes, linear)
[ 1.288614] NET: Registered protocol family 1
[ 1.289675] RPC: Registered named UNIX socket transport module.
[ 1.289688] RPC: Registered udp transport module.
[ 1.289692] RPC: Registered tcp transport module.
[ 1.289696] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 1.289713] NET: Registered protocol family 44
[ 1.292430] Initialise system trusted keyrings
[ 1.292871] workingset: timestamp_bits=14 max_order=17 bucket_order=3
[ 1.301101] zbud: loaded
[ 1.305051] NFS: Registering the id_resolver key type
[ 1.305115] Key type id_resolver registered
[ 1.305121] Key type id_legacy registered
[ 1.305285] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 1.305296] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 1.305677] fuse: init (API version 7.32)
[ 1.399238] xor: automatically using best checksumming function neon
[ 1.399258] Key type asymmetric registered
[ 1.399266] Asymmetric key parser 'x509' registered
[ 1.399340] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 1.399934] io scheduler mq-deadline registered
[ 1.403387] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 1.408534] l3-aon-clkctrl:0000:0: failed to disable
[ 1.412175] Serial: 8250/16550 driver, 6 ports, IRQ sharing disabled
[ 1.420965] CAN device driver interface
[ 1.421588] usbcore: registered new interface driver smsc95xx
[ 1.422213] usbcore: registered new interface driver uas
[ 1.422278] usbcore: registered new interface driver usb-storage
[ 1.422315] usbcore: registered new interface driver ums-alauda
[ 1.422348] usbcore: registered new interface driver ums-cypress
[ 1.422381] usbcore: registered new interface driver ums-datafab
[ 1.422414] usbcore: registered new interface driver ums_eneub6250
[ 1.422448] usbcore: registered new interface driver ums-freecom
[ 1.422480] usbcore: registered new interface driver ums-isd200
[ 1.422512] usbcore: registered new interface driver ums-jumpshot
[ 1.422581] usbcore: registered new interface driver ums-karma
[ 1.422619] usbcore: registered new interface driver ums-onetouch
[ 1.422669] usbcore: registered new interface driver ums-realtek
[ 1.422704] usbcore: registered new interface driver ums-sddr09
[ 1.422738] usbcore: registered new interface driver ums-sddr55
[ 1.422771] usbcore: registered new interface driver ums-usbat
[ 1.425085] i2c /dev entries driver
[ 1.425255] Driver for 1-wire Dallas network protocol.
[ 1.426444] softdog: initialized. soft_noboot=0 soft_margin=60 sec soft_panic=0 (nowayout=0)
[ 1.426457] softdog: soft_reboot_cmd=<not set> soft_active_on_boot=0
[ 1.427811] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.428527] sdhci: Secure Digital Host Controller Interface driver
[ 1.428535] sdhci: Copyright(c) Pierre Ossman
[ 1.428723] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.429503] hid: raw HID events driver (C) Jiri Kosina
[ 1.429893] usbcore: registered new interface driver usbhid
[ 1.429901] usbhid: USB HID core driver
[ 1.430532] drop_monitor: Initializing network drop monitor service
[ 1.431936] NET: Registered protocol family 10
[ 1.437140] Segment Routing with IPv6
[ 1.437266] mip6: Mobile IPv6
[ 1.437278] NET: Registered protocol family 17
[ 1.437310] can: controller area network core
[ 1.437404] NET: Registered protocol family 29
[ 1.437901] Key type dns_resolver registered
[ 1.437915] mpls_gso: MPLS GSO support
[ 1.438204] ThumbEE CPU extension supported.
[ 1.438222] Registering SWP/SWPB emulation handler
[ 1.438231] omap_voltage_late_init: Voltage driver support not added
[ 1.438516] PM: Cannot get wkup_m3_ipc handle
[ 1.439274] registered taskstats version 1
[ 1.439299] Loading compiled-in X.509 certificates
[ 1.439438] zswap: loaded using pool lzo/zbud
[ 1.440433] Key type .fscrypt registered
[ 1.440445] Key type fscrypt-provisioning registered
[ 1.445448] Btrfs loaded, crc32c=crc32c-generic
[ 1.445647] AppArmor: AppArmor sha1 policy hashing enabled
[ 1.512329] wkup_m3_rproc 44d00000.cpu: Platform data missing!
[ 1.581318] gpiochip_add_data_with_key: GPIOs 0..31 (gpio-0-31) failed to register, -517
[ 1.749224] pinctrl-single 44e10800.pinmux: 142 pins, size 568
[ 1.856338] wkup_m3_ipc 44e11324.wkup_m3_ipc: IPC Request for A8->M3 Channel failed! -517
[ 1.904466] ti-sysc: probe of 44e31000.target-module failed with error -16
[ 1.950359] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.996115] omap_rtc 44e3e000.rtc: registered as rtc1
[ 2.039963] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 25, base_baud = 3000000) is a 8250
[ 2.063459] 48024000.serial: ttyS2 at MMIO 0x48024000 (irq = 26, base_baud = 3000000) is a 8250
[ 2.125693] rtc-pcf8563 1-0051: registered as rtc0
[ 2.126961] rtc-pcf8563 1-0051: setting system clock to 2023-11-02T05:57:34 UTC (1698904654)
[ 2.128247] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 100 kHz
[ 2.182033] ti-sysc: probe of 48040000.target-module failed with error -16
[ 2.313108] OMAP GPIO hardware version 0.1
[ 2.369181] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 2.401616] at24 2-0054: supply vcc not found, using dummy regulator
[ 2.436067] at24 2-0055: supply vcc not found, using dummy regulator
[ 2.470807] at24 2-0056: supply vcc not found, using dummy regulator
[ 2.502737] at24 2-0057: supply vcc not found, using dummy regulator
[ 2.529960] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 100 kHz
[ 2.552595] 481a6000.serial: ttyS3 at MMIO 0x481a6000 (irq = 39, base_baud = 3000000) is a 8250
[ 2.565037] 481a8000.serial: ttyS4 at MMIO 0x481a8000 (irq = 40, base_baud = 3000000) is a 8250
[ 2.577271] 481aa000.serial: ttyS5 at MMIO 0x481aa000 (irq = 41, base_baud = 3000000) is a 8250
[ 2.612040] c_can_platform 481cc000.can: c_can_platform device registered (regs=(ptrval), irq=44)
[ 2.623549] c_can_platform 481d0000.can: c_can_platform device registered (regs=(ptrval), irq=45)
[ 2.636155] sdhci-omap 481d8000.mmc: supply vqmmc not found, using dummy regulator
[ 2.732772] omap_rng 48310000.rng: Random Number Generator ver. 20
[ 2.736011] random: crng init done
[ 2.783770] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 2.784073] mdio_bus 4a101000.mdio: MDIO device at address 0 is missing.
[ 2.784703] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 2.784719] cpsw 4a100000.ethernet: ALE Table size 1024
[ 2.784824] cpsw 4a100000.ethernet: cpts: overflow check period 1250 (jiffies)
[ 2.784892] cpsw 4a100000.ethernet: Detected MACID = 60:e8:5b:e3:91:53
[ 2.806562] debugfs: Directory '49000000.dma' with parent 'dmaengine' already present!
[ 2.806594] edma 49000000.dma: TI EDMA DMA engine driver
[ 2.816389] am335x-phy-driver 47401300.usb-phy: supply vcc not found, using dummy regulator
[ 2.816744] am335x-phy-driver 47401300.usb-phy: dummy supplies not allowed for exclusive requests
[ 2.828821] am335x-phy-driver 47401b00.usb-phy: supply vcc not found, using dummy regulator
[ 2.829148] am335x-phy-driver 47401b00.usb-phy: dummy supplies not allowed for exclusive requests
[ 2.835434] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 2.835476] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 2.835923] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10
[ 2.835939] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.835948] usb usb1: Product: MUSB HDRC host driver
[ 2.835955] usb usb1: Manufacturer: Linux 5.10.186-bone-rt-r76 musb-hcd
[ 2.835962] usb usb1: SerialNumber: musb-hdrc.1
[ 2.836805] hub 1-0:1.0: USB hub found
[ 2.836875] hub 1-0:1.0: 1 port detected
[ 2.859666] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 2.860381] omap-sham 53100000.sham: will run requests pump with realtime priority
[ 2.866146] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 2.866792] omap-aes 53500000.aes: will run requests pump with realtime priority
[ 3.017238] gpio-of-helper ocp:cape-universal: Allocated GPIO id=0 name='P8_03'
[ 3.017478] gpio-of-helper ocp:cape-universal: Allocated GPIO id=1 name='P8_04'
[ 3.017672] gpio-of-helper ocp:cape-universal: Allocated GPIO id=2 name='P8_05'
[ 3.017847] gpio-of-helper ocp:cape-universal: Allocated GPIO id=3 name='P8_06'
[ 3.018239] gpio-of-helper ocp:cape-universal: Allocated GPIO id=4 name='P8_07'
[ 3.018430] gpio-of-helper ocp:cape-universal: Allocated GPIO id=5 name='P8_08'
[ 3.018612] gpio-of-helper ocp:cape-universal: Allocated GPIO id=6 name='P8_09'
[ 3.018785] gpio-of-helper ocp:cape-universal: Allocated GPIO id=7 name='P8_10'
[ 3.018950] gpio-of-helper ocp:cape-universal: Allocated GPIO id=8 name='P8_11'
[ 3.019126] gpio-of-helper ocp:cape-universal: Allocated GPIO id=9 name='P8_12'
[ 3.019173] gpio-of-helper ocp:cape-universal: Failed to get gpio property of 'P8_13'
[ 3.019181] gpio-of-helper ocp:cape-universal: Failed to create gpio entry
[ 3.023489] PM: Cannot get wkup_m3_ipc handle
[ 3.026808] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 19, base_baud = 3000000) is a 8250
[ 3.027834] printk: console [ttyS0]: printing thread started
[ 3.027857] printk: console [ttyS0] enabled
[ 3.066299] tps65217-pmic: Failed to locate of_node [id: -1]
[ 3.101788] tps65217-bl: Failed to locate of_node [id: -1]
[ 3.104762] tps6521x_pwrbutton tps65217-pwrbutton: DMA mask not set
[ 3.105853] input: tps65217_pwr_but as /devices/platform/ocp/44c00000.interconnect/44c00000.interconnect:segment@200000/44e0b000.target-module/44e0b000.i2c/i2c-0/0-0024/tps65217-pwrbutton/input/input0
[ 3.114379] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[ 3.116179] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 3.116420] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 3.117324] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 3.122201] omap_gpio 44e07000.gpio: Could not set line 6 debounce to 200000 microseconds (-22)
[ 3.122226] sdhci-omap 48060000.mmc: Got CD GPIO
[ 3.122430] sdhci-omap 48060000.mmc: supply vqmmc not found, using dummy regulator
[ 3.133193] sdhci-omap 481d8000.mmc: supply vqmmc not found, using dummy regulator
[ 3.144645] gpio-of-helper ocp:cape-universal: Allocated GPIO id=0 name='P8_03'
[ 3.144815] gpio-of-helper ocp:cape-universal: Allocated GPIO id=1 name='P8_04'
[ 3.144943] gpio-of-helper ocp:cape-universal: Allocated GPIO id=2 name='P8_05'
[ 3.145065] gpio-of-helper ocp:cape-universal: Allocated GPIO id=3 name='P8_06'
[ 3.145489] gpio-of-helper ocp:cape-universal: Allocated GPIO id=4 name='P8_07'
[ 3.145625] gpio-of-helper ocp:cape-universal: Allocated GPIO id=5 name='P8_08'
[ 3.145770] gpio-of-helper ocp:cape-universal: Allocated GPIO id=6 name='P8_09'
[ 3.145903] gpio-of-helper ocp:cape-universal: Allocated GPIO id=7 name='P8_10'
[ 3.146036] gpio-of-helper ocp:cape-universal: Allocated GPIO id=8 name='P8_11'
[ 3.146168] gpio-of-helper ocp:cape-universal: Allocated GPIO id=9 name='P8_12'
[ 3.146404] gpio-of-helper ocp:cape-universal: Allocated GPIO id=10 name='P8_13'
[ 3.146588] gpio-of-helper ocp:cape-universal: Allocated GPIO id=11 name='P8_14'
[ 3.146766] gpio-of-helper ocp:cape-universal: Allocated GPIO id=12 name='P8_15'
[ 3.146930] gpio-of-helper ocp:cape-universal: Allocated GPIO id=13 name='P8_16'
[ 3.147109] gpio-of-helper ocp:cape-universal: Allocated GPIO id=14 name='P8_17'
[ 3.147286] gpio-of-helper ocp:cape-universal: Allocated GPIO id=15 name='P8_18'
[ 3.147449] gpio-of-helper ocp:cape-universal: Allocated GPIO id=16 name='P8_19'
[ 3.147635] gpio-of-helper ocp:cape-universal: Allocated GPIO id=17 name='P8_20'
[ 3.148050] gpio-of-helper ocp:cape-universal: Allocated GPIO id=18 name='P8_21'
[ 3.148233] gpio-of-helper ocp:cape-universal: Allocated GPIO id=19 name='P8_22'
[ 3.148419] gpio-of-helper ocp:cape-universal: Allocated GPIO id=20 name='P8_23'
[ 3.148582] gpio-of-helper ocp:cape-universal: Allocated GPIO id=21 name='P8_24'
[ 3.148772] gpio-of-helper ocp:cape-universal: Allocated GPIO id=22 name='P8_25'
[ 3.148944] gpio-of-helper ocp:cape-universal: Allocated GPIO id=23 name='P8_26'
[ 3.149113] gpio-of-helper ocp:cape-universal: Allocated GPIO id=24 name='P8_27'
[ 3.149289] gpio-of-helper ocp:cape-universal: Allocated GPIO id=25 name='P8_28'
[ 3.149454] gpio-of-helper ocp:cape-universal: Allocated GPIO id=26 name='P8_29'
[ 3.149623] gpio-of-helper ocp:cape-universal: Allocated GPIO id=27 name='P8_30'
[ 3.149802] gpio-of-helper ocp:cape-universal: Allocated GPIO id=28 name='P8_31'
[ 3.149986] gpio-of-helper ocp:cape-universal: Allocated GPIO id=29 name='P8_32'
[ 3.150174] gpio-of-helper ocp:cape-universal: Allocated GPIO id=30 name='P8_33'
[ 3.150340] gpio-of-helper ocp:cape-universal: Allocated GPIO id=31 name='P8_34'
[ 3.150510] gpio-of-helper ocp:cape-universal: Allocated GPIO id=32 name='P8_35'
[ 3.150679] gpio-of-helper ocp:cape-universal: Allocated GPIO id=33 name='P8_36'
[ 3.150843] gpio-of-helper ocp:cape-universal: Allocated GPIO id=34 name='P8_37'
[ 3.151015] gpio-of-helper ocp:cape-universal: Allocated GPIO id=35 name='P8_38'
[ 3.151177] gpio-of-helper ocp:cape-universal: Allocated GPIO id=36 name='P8_39'
[ 3.151348] gpio-of-helper ocp:cape-universal: Allocated GPIO id=37 name='P8_40'
[ 3.151543] gpio-of-helper ocp:cape-universal: Allocated GPIO id=38 name='P8_41'
[ 3.156927] mmc0: SDHCI controller on 48060000.mmc [48060000.mmc] using External DMA
[ 3.157512] gpio-of-helper ocp:cape-universal: Allocated GPIO id=39 name='P8_42'
[ 3.157741] gpio-of-helper ocp:cape-universal: Allocated GPIO id=40 name='P8_43'
[ 3.157928] gpio-of-helper ocp:cape-universal: Allocated GPIO id=41 name='P8_44'
[ 3.158094] gpio-of-helper ocp:cape-universal: Allocated GPIO id=42 name='P8_45'
[ 3.158273] gpio-of-helper ocp:cape-universal: Allocated GPIO id=43 name='P8_46'
[ 3.158459] gpio-of-helper ocp:cape-universal: Allocated GPIO id=44 name='P9_11'
[ 3.158656] gpio-of-helper ocp:cape-universal: Allocated GPIO id=45 name='P9_12'
[ 3.158844] gpio-of-helper ocp:cape-universal: Allocated GPIO id=46 name='P9_13'
[ 3.159011] gpio-of-helper ocp:cape-universal: Allocated GPIO id=47 name='P9_14'
[ 3.159190] gpio-of-helper ocp:cape-universal: Allocated GPIO id=48 name='P9_15'
[ 3.159386] gpio-of-helper ocp:cape-universal: Allocated GPIO id=49 name='P9_16'
[ 3.159561] gpio-of-helper ocp:cape-universal: Allocated GPIO id=50 name='P9_17'
[ 3.159853] gpio-of-helper ocp:cape-universal: Allocated GPIO id=51 name='P9_18'
[ 3.160035] gpio-of-helper ocp:cape-universal: Allocated GPIO id=52 name='P9_19'
[ 3.160218] gpio-of-helper ocp:cape-universal: Allocated GPIO id=53 name='P9_20'
[ 3.160396] gpio-of-helper ocp:cape-universal: Allocated GPIO id=54 name='P9_21'
[ 3.160562] gpio-of-helper ocp:cape-universal: Allocated GPIO id=55 name='P9_22'
[ 3.160742] gpio-of-helper ocp:cape-universal: Allocated GPIO id=56 name='P9_23'
[ 3.160911] gpio-of-helper ocp:cape-universal: Allocated GPIO id=57 name='P9_24'
[ 3.161468] gpio-of-helper ocp:cape-universal: Allocated GPIO id=58 name='P9_25'
[ 3.161668] gpio-of-helper ocp:cape-universal: Allocated GPIO id=59 name='P9_26'
[ 3.161844] gpio-of-helper ocp:cape-universal: Allocated GPIO id=60 name='P9_27'
[ 3.162018] gpio-of-helper ocp:cape-universal: Allocated GPIO id=61 name='P9_28'
[ 3.162196] gpio-of-helper ocp:cape-universal: Allocated GPIO id=62 name='P9_29'
[ 3.162372] gpio-of-helper ocp:cape-universal: Allocated GPIO id=63 name='P9_30'
[ 3.162547] gpio-of-helper ocp:cape-universal: Allocated GPIO id=64 name='P9_31'
[ 3.162717] gpio-of-helper ocp:cape-universal: Allocated GPIO id=65 name='P9_41'
[ 3.162892] gpio-of-helper ocp:cape-universal: Allocated GPIO id=66 name='P9_91'
[ 3.163087] gpio-of-helper ocp:cape-universal: Allocated GPIO id=67 name='P9_42'
[ 3.163258] gpio-of-helper ocp:cape-universal: Allocated GPIO id=68 name='P9_92'
[ 3.163269] gpio-of-helper ocp:cape-universal: ready
[ 3.170634] mmc1: SDHCI controller on 481d8000.mmc [481d8000.mmc] using External DMA
[ 3.173389] PM: Cannot get wkup_m3_ipc handle
[ 3.174234] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 3.179819] PM: Cannot get wkup_m3_ipc handle
[ 3.180299] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 3.185555] Waiting for root device /dev/mmcblk0p1...
[ 3.261656] mmc1: new high speed MMC card at address 0001
[ 3.263122] mmcblk1: mmc1:0001 Q2J55L 7.09 GiB
[ 3.263827] mmcblk1boot0: mmc1:0001 Q2J55L partition 1 16.0 MiB
[ 3.264224] mmcblk1boot1: mmc1:0001 Q2J55L partition 2 16.0 MiB
[ 3.264568] mmcblk1rpmb: mmc1:0001 Q2J55L partition 3 4.00 MiB, chardev (242:0)
[ 3.266788] mmcblk1: p1 p2 p3 p4
[ 3.269374] mmc0: new high speed SDHC card at address aaaa
[ 3.270660] mmcblk0: mmc0:aaaa SP32G 29.7 GiB
[ 3.273008] mmcblk0: p1
[ 3.284541] PM: Cannot get wkup_m3_ipc handle
[ 3.285147] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 3.312404] PM: Cannot get wkup_m3_ipc handle
[ 3.312974] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 3.337145] EXT4-fs (mmcblk0p1): INFO: recovery required on readonly filesystem
[ 3.337168] EXT4-fs (mmcblk0p1): write access will be enabled during recovery
[ 3.359757] usb 1-1: new high-speed USB device number 2 using musb-hdrc
[ 3.421210] EXT4-fs (mmcblk0p1): recovery complete
[ 3.423112] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Opts: (null)
[ 3.423238] VFS: Mounted root (ext4 filesystem) readonly on device 179:769.
[ 3.431665] devtmpfs: mounted
[ 3.440099] Freeing unused kernel memory: 1024K
[ 3.440730] Run /sbin/init as init process
[ 3.440739] with arguments:
[ 3.440745] /sbin/init
[ 3.440750] with environment:
[ 3.440755] HOME=/
[ 3.440759] TERM=linux
[ 3.471424] Not activating Mandatory Access Control as /sbin/tomoyo-init does not exist.
[ 3.508517] usb 1-1: New USB device found, idVendor=0424, idProduct=2806, bcdDevice= 6.24
[ 3.508547] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 3.508556] usb 1-1: Product: USB2806 Smart Hub
[ 3.508564] usb 1-1: Manufacturer: Microchip
[ 3.510043] hub 1-1:1.0: USB hub found
[ 3.510144] hub 1-1:1.0: 7 ports detected
[ 3.512217] PM: Cannot get wkup_m3_ipc handle
[ 3.512800] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 4.141252] systemd[1]: systemd 247.3-7+deb11u1 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +ZSTD +SECCOMP +BLKID +ELFUTILS +KMOD +IDN2 -IDN +PCRE2 default-hierarchy=unified)
[ 4.142136] systemd[1]: Detected architecture arm.
[ 4.145339] systemd[1]: Set hostname to <STU>.
[ 4.219760] usb 1-1.5: new high-speed USB device number 3 using musb-hdrc
[ 4.320471] usb 1-1.5: New USB device found, idVendor=0424, idProduct=7850, bcdDevice= 3.00
[ 4.320503] usb 1-1.5: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 4.320513] usb 1-1.5: Product: LAN7850
[ 4.320521] usb 1-1.5: Manufacturer: Microchip
[ 4.320528] usb 1-1.5: SerialNumber: 00800F785000
[ 4.322595] PM: Cannot get wkup_m3_ipc handle
[ 4.323188] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 4.407889] usb 1-1.6: new high-speed USB device number 4 using musb-hdrc
[ 4.508436] usb 1-1.6: New USB device found, idVendor=0424, idProduct=7850, bcdDevice= 3.00
[ 4.508468] usb 1-1.6: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 4.508479] usb 1-1.6: Product: LAN7850
[ 4.508486] usb 1-1.6: Manufacturer: Microchip
[ 4.508493] usb 1-1.6: SerialNumber: 00800F785000
[ 4.510565] PM: Cannot get wkup_m3_ipc handle
[ 4.511162] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 4.587849] usb 1-1.7: new high-speed USB device number 5 using musb-hdrc
[ 4.688996] usb 1-1.7: New USB device found, idVendor=0424, idProduct=2840, bcdDevice= 2.04
[ 4.689029] usb 1-1.7: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 4.689040] usb 1-1.7: Product: Hub Feature Controller
[ 4.689047] usb 1-1.7: Manufacturer: Microchip
[ 4.690729] PM: Cannot get wkup_m3_ipc handle
[ 4.691313] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 5.525165] systemd[1]: Queued start job for default target Graphical Interface.
[ 5.533174] systemd[1]: Created slice system-getty.slice.
[ 5.536542] systemd[1]: Created slice system-modprobe.slice.
[ 5.539397] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ 5.542183] systemd[1]: Created slice User and Session Slice.
[ 5.542991] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ 5.543532] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ 5.545507] systemd[1]: Set up automount Arbitrary Executable File Formats File System Automount Point.
[ 5.545971] systemd[1]: Reached target Local Encrypted Volumes.
[ 5.546439] systemd[1]: Reached target Paths.
[ 5.546669] systemd[1]: Reached target Remote File Systems.
[ 5.546805] systemd[1]: Reached target Slices.
[ 5.547065] systemd[1]: Reached target Swap.
[ 5.559198] systemd[1]: Listening on Syslog Socket.
[ 5.560680] systemd[1]: Listening on fsck to fsckd communication Socket.
[ 5.561422] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ 5.563000] systemd[1]: Listening on Journal Audit Socket.
[ 5.564365] systemd[1]: Listening on Journal Socket (/dev/log).
[ 5.565697] systemd[1]: Listening on Journal Socket.
[ 5.567157] systemd[1]: Listening on udev Control Socket.
[ 5.568480] systemd[1]: Listening on udev Kernel Socket.
[ 5.569847] systemd[1]: Condition check resulted in Huge Pages File System being skipped.
[ 5.577510] systemd[1]: Mounting POSIX Message Queue File System...
[ 5.591652] systemd[1]: Mounting Kernel Debug File System...
[ 5.627172] systemd[1]: Mounting Kernel Trace File System...
[ 5.673602] systemd[1]: Starting Restore / save the current clock...
[ 5.752844] systemd[1]: Starting Create list of static device nodes for the current kernel...
[ 5.788523] systemd[1]: Starting Load Kernel Module configfs...
[ 5.813325] systemd[1]: Starting Load Kernel Module drm...
[ 5.849629] systemd[1]: Starting Load Kernel Module fuse...
[ 5.861903] systemd[1]: Condition check resulted in Set Up Additional Binary Formats being skipped.
[ 5.886249] systemd[1]: Starting File System Check on Root Device...
[ 5.926380] systemd[1]: Starting Journal Service...
[ 5.969216] systemd[1]: Starting Load Kernel Modules...
[ 6.009355] systemd[1]: Starting Coldplug All udev Devices...
[ 6.108499] systemd[1]: Mounted POSIX Message Queue File System.
[ 6.110004] systemd[1]: Mounted Kernel Debug File System.
[ 6.111099] systemd[1]: Mounted Kernel Trace File System.
[ 6.138829] systemd[1]: Finished Restore / save the current clock.
[ 6.164205] systemd[1]: Finished Create list of static device nodes for the current kernel.
[ 6.167239] systemd[1]: modprobe@configfs.service: Succeeded.
[ 6.195159] systemd[1]: Finished Load Kernel Module configfs.
[ 6.222794] systemd[1]: modprobe@drm.service: Succeeded.
[ 6.248390] systemd[1]: Finished Load Kernel Module drm.
[ 6.251649] systemd[1]: modprobe@fuse.service: Succeeded.
[ 6.272627] systemd[1]: Finished Load Kernel Module fuse.
[ 6.343828] systemd[1]: Mounting FUSE Control File System...
[ 6.429722] systemd[1]: Mounting Kernel Configuration File System...
[ 6.501012] systemd[1]: Started File System Check Daemon to report status.
[ 6.619994] systemd[1]: Finished File System Check on Root Device.
[ 6.636278] systemd[1]: Finished Load Kernel Modules.
[ 6.637996] systemd[1]: Mounted FUSE Control File System.
[ 6.639112] systemd[1]: Mounted Kernel Configuration File System.
[ 6.685229] systemd[1]: Starting Remount Root and Kernel File Systems...
[ 6.733292] systemd[1]: Starting Apply Kernel Variables...
[ 7.008211] systemd[1]: Finished Apply Kernel Variables.
[ 7.020368] EXT4-fs (mmcblk0p1): re-mounted. Opts: errors=remount-ro
[ 7.052360] systemd[1]: Finished Remount Root and Kernel File Systems.
[ 7.058962] systemd[1]: Condition check resulted in Rebuild Hardware Database being skipped.
[ 7.059443] systemd[1]: Condition check resulted in Platform Persistent Storage Archival being skipped.
[ 7.077464] systemd[1]: Starting Load/Save Random Seed...
[ 7.110514] systemd[1]: Starting Create System Users...
[ 7.368059] systemd[1]: Finished Load/Save Random Seed.
[ 7.369589] systemd[1]: Condition check resulted in First Boot Complete being skipped.
[ 7.448323] systemd[1]: Finished Create System Users.
[ 7.473327] systemd[1]: Starting Create Static Device Nodes in /dev...
[ 7.764757] systemd[1]: Finished Create Static Device Nodes in /dev.
[ 7.765897] systemd[1]: Reached target Local File Systems (Pre).
[ 7.766096] systemd[1]: Reached target Local File Systems.
[ 7.766472] systemd[1]: Condition check resulted in Store a System Token in an EFI Variable being skipped.
[ 7.766785] systemd[1]: Condition check resulted in Commit a transient machine-id on disk being skipped.
[ 7.803473] systemd[1]: Starting Rule-based Manager for Device Events and Files...
[ 8.500304] systemd[1]: Started Journal Service.
[ 8.801386] systemd-journald[230]: Received client request to flush runtime journal.
[ 19.044588] PM: Cannot get wkup_m3_ipc handle
[ 19.045219] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 19.067381] PM: Cannot get wkup_m3_ipc handle
[ 19.068157] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 19.080392] PM: Cannot get wkup_m3_ipc handle
[ 19.081017] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 19.097171] PM: Cannot get wkup_m3_ipc handle
[ 19.098011] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 19.604688] PM: Cannot get wkup_m3_ipc handle
[ 19.605311] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 19.874090] PM: Cannot get wkup_m3_ipc handle
[ 19.874708] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 20.148413] PM: Cannot get wkup_m3_ipc handle
[ 20.149051] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 20.612775] PM: Cannot get wkup_m3_ipc handle
[ 20.613388] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 20.614066] usbcore: registered new interface driver lan78xx
[ 22.133390] PM: Cannot get wkup_m3_ipc handle
[ 22.133986] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 22.161546] PM: Cannot get wkup_m3_ipc handle
[ 22.162137] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 22.189431] PM: Cannot get wkup_m3_ipc handle
[ 22.190015] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 26.588886] lan78xx 1-1.5:1.0 eth3: renamed from eth1
[ 26.644215] lan78xx 1-1.6:1.0 eth4: renamed from eth2
There are so many failure messages like wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle…
I can’t manage to enable GPIOs with the same configuration worked in the previous kernel…
Could you please give me some advises?
Thank you in advance!