This is a page about Samsung’s ARTIK 5 Kit.
Availability
Boards:
- ARTIK 5 at DigiKey
Basic Requirements
- Running a recent supported release of Debian, Fedora or Ubuntu on a x86 64bit based PC; without OS Virtualization Software.
- Many of the listed commands assume /bin/bash as the default shell.
- ARM Cross Compiler – Linaro: https://www.linaro.org
- Linaro Toolchain Binaries: https://www.linaro.org/downloads/
- Bootloader
- Das U-Boot – the Universal Boot Loader: http://www.denx.de/wiki/U-Boot
- Source: https://github.com/u-boot/u-boot/
- Linux Kernel
- Linus’s Mainline tree: https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git
- ARM based rootfs
- Debian: https://www.debian.org
Linux Kernel
This script will build the kernel, modules, device tree binaries and copy them to the deploy directory.
Download:
#user@localhost:~$
git clone https://github.com/RobertCNelson/armv7_devel ./kernelbuildscripts
cd kernelbuildscripts/
For v4.9.x-artik-armv7 (Longterm 4.9.x):
#user@localhost:~/kernelbuildscripts$
git checkout origin/v4.9.x-artik-armv7 -b tmp
For v4.14.x-artik-armv7 (Longterm 4.14.x):
#user@localhost:~/kernelbuildscripts$
git checkout origin/v4.14.x-artik-armv7 -b tmp
For v4.15.x-artik-armv7 (Prepatch):
#user@localhost:~/kernelbuildscripts$
git checkout origin/v4.15.x-artik-armv7 -b tmp
Build:
#user@localhost:~/kernelbuildscripts$
./build_kernel.sh
Root File System
Debian 11
| User | Password |
|---|---|
| debian | temppwd |
| root | root |
Download:
#user@localhost:~$
wget -c https://rcn-ee.com/rootfs/eewiki/minfs/debian-11.3-minimal-armhf-2022-04-15.tar.xz
Verify:
#user@localhost:~$
sha256sum debian-11.3-minimal-armhf-2022-04-15.tar.xz
#sha256sum output:
575738843651de2962f251447f4742d4f33313d6f7f5edf282a401207f5e6646 debian-11.3-minimal-armhf-2022-04-15.tar.xz
Extract:
#user@localhost:~$
tar xf debian-11.3-minimal-armhf-2022-04-15.tar.xz
Setup microSD card
We need to access the External Drive to be utilized by the target device. Run lsblk to help figure out what linux device has been reserved for your External Drive.
#Example: for DISK=/dev/sdX
lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT
sda 8:0 0 465.8G 0 disk
├─sda1 8:1 0 512M 0 part /boot/efi
└─sda2 8:2 0 465.3G 0 part / <- Development Machine Root Partition
sdb 8:16 1 962M 0 disk <- microSD/USB Storage Device
└─sdb1 8:17 1 961M 0 part <- microSD/USB Storage Partition
#Thus you would use:
export DISK=/dev/sdb
#Example: for DISK=/dev/mmcblkX
lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT
sda 8:0 0 465.8G 0 disk
├─sda1 8:1 0 512M 0 part /boot/efi
└─sda2 8:2 0 465.3G 0 part / <- Development Machine Root Partition
mmcblk0 179:0 0 962M 0 disk <- microSD/USB Storage Device
└─mmcblk0p1 179:1 0 961M 0 part <- microSD/USB Storage Partition
#Thus you would use:
export DISK=/dev/mmcblk0
Erase partition table/labels on microSD card:
sudo dd if=/dev/zero of=${DISK} bs=1M count=100
Install Bootloader:
#user@localhost:~$
wget -c https://rcn-ee.com/repos/git/build-artik/prebuilt/artik5/bl1.bin
sudo dd if=./bl1.bin of=${DISK} seek=1 bs=512
wget -c https://rcn-ee.com/repos/git/build-artik/prebuilt/artik5/bl2.bin
sudo dd if=./bl2.bin of=${DISK} seek=31 bs=512
wget -c https://rcn-ee.com/repos/bootloader/artik5/u-boot-artik5-v2012.07-r3.bin
sudo dd if=./u-boot-artik5-v2012.07-r3.bin of=${DISK} seek=63 bs=512
wget -c https://rcn-ee.com/repos/git/build-artik/prebuilt/artik5/tzsw.bin
sudo dd if=./tzsw.bin of=${DISK} seek=719 bs=512
Create Partition Layout:
With util-linux v2.26, sfdisk was rewritten and is now based on libfdisk.
#Check the version of sfdisk installed on your pc is atleast 2.26.x or newer.
sudo sfdisk --version
#Example Output
sfdisk from util-linux 2.27.1
#sfdisk >= 2.26.x
sudo sfdisk ${DISK} <<-__EOF__
1M,48M,0xE,*
,,,-
__EOF__
Format Partition:
With mkfs.ext4 1.43, we need to make sure metadata_csum and 64bit ext4 features are disabled.
As the version of U-Boot needed for this target CAN NOT correctly handle reading files with these newer ext4 options.
#mkfs.ext4 -V
sudo mkfs.ext4 -V
mke2fs 1.43-WIP (15-Mar-2016)
Using EXT2FS Library version 1.43-WIP
#mkfs.ext4 >= 1.43
for: DISK=/dev/mmcblkX
sudo mkfs.vfat -F 16 -n BOOT ${DISK}p1
sudo mkfs.ext4 -L rootfs -O ^metadata_csum,^64bit ${DISK}p2
for: DISK=/dev/sdX
sudo mkfs.vfat -F 16 -n BOOT ${DISK}1
sudo mkfs.ext4 -L rootfs -O ^metadata_csum,^64bit ${DISK}2
Mount Partition:
On most systems these partitions may be auto-mounted…
sudo mkdir -p /media/boot/
sudo mkdir -p /media/rootfs/
for: DISK=/dev/mmcblkX
sudo mount ${DISK}p1 /media/boot/
sudo mount ${DISK}p2 /media/rootfs/
for: DISK=/dev/sdX
sudo mount ${DISK}1 /media/boot/
sudo mount ${DISK}2 /media/rootfs/
uEnv.txt script
Not used yet…
#~/
sudo touch /media/boot/uEnv.txt
Install Kernel and Root File System
To help new users, since the kernel version can change on a daily basis. The kernel building scripts listed on this page will now give you a hint of what kernel version was built.
-----------------------------
Script Complete
eewiki.net: [user@localhost:~$ export kernel_version=5.X.Y-Z]
-----------------------------
Copy and paste that “export kernel_version=5.X.Y-Z” exactly as shown in your own build/desktop environment and hit enter to create an environment variable to be used later.
export kernel_version=5.X.Y-Z
Copy Root File System
#Debian; Root File System: user@localhost:~$
sudo tar xfvp ./debian-*-*-armhf-*/armhf-rootfs-*.tar -C /media/rootfs/
sync
Copy Kernel Image
Kernel Image:
#user@localhost:~$
sudo cp -v ./kernelbuildscripts/deploy/${kernel_version}.zImage /media/boot/zImage
Copy Kernel Device Tree Binaries
#user@localhost:~$
sudo mkdir -p /media/boot/dtbs/
sudo tar xfvo ./kernelbuildscripts/deploy/${kernel_version}-dtbs.tar.gz -C /media/boot/dtbs/
Copy Kernel Modules
#user@localhost:~$
sudo tar xfv ./kernelbuildscripts/deploy/${kernel_version}-modules.tar.gz -C /media/rootfs/
File Systems Table (/etc/fstab)
#user@localhost:~/$
sudo sh -c "echo '/dev/mmcblk1p2 / auto errors=remount-ro 0 1' >> /media/rootfs/etc/fstab"
sudo sh -c "echo '/dev/mmcblk1p1 /boot/uboot auto defaults 0 2' >> /media/rootfs/etc/fstab"
Remove microSD/SD card
sync
sudo umount /media/boot
sudo umount /media/rootfs
Comments
Any questions or comments please go to our TechForum: TechForum