DigiKey Part Number 277-17838-ND Voltage Rating

Hi, I have a question in regards this specific [Circuit Protection]

1019998 Phoenix Contact | Circuit Protection | DigiKey

Voltage Rating - DC 125 V

What is meant by this voltage rating? Is the maximum operating voltage meant here?

Does this item have a defined range of operation, for example, 12 to 125 VDC?

If yes, will circuit breaker protection be full effective within this changeable range of operation?

Thanks,
JJ Pina

Hello @jose.pina

Welcome to the TechForum

Yes, you are correct, the voltage rating is the max voltage the circuit breaker can tolerate before damage will be done to the circuit breaker.
There is no defined range of operations for the voltage as long as you are at or below the circuit breaker voltage rating as the circuit breaker is looking for a surge in the current above its current rating.

I have included a few TechForum post that can explain more about circuit breakers attributes and their operation.
Circuit Breakers - Resources / Product Selection Guide, DigiKey TechForum

Circuit breakers, DigiKey TechForum

What’s inside a circuit breaker? An introduction to the thermal and magnetic trip, DigiKey TechForum

Thank you very much!

JJ Pina