DKRed: An extension of DigiKey's PCB Builder

Hi @maalikKyzer! I got in touch with the board house. They provided another updated document that shows the Df and Dr values. I’m going to edit my previous posts to show this file, but here it is:

DKRed - 4 layer Stackup v2.pdf (392.8 KB)

As for your second question, the boardhouse said, “Tg is an attribute which 370HR meets.”

Thank you again for your questions on these. I apologize for all the revisions but want to get this right with all the information needed.

No worries @Linzee_1029 . Thanks for the update.
One final question. Board houses tend to provide impedance trace recommendations.

Using Altium, when using the 4 layer PCB stackup info, I calculated two impedance profiles for

  • 50 Ohm, 2.4GHz coplanar waveguide = 8.941mil width and 5mil clearance
  • 90 Ohm, USB 2 differential coplanar = 6.947mil width and 5 mil clearance

as shown in the attached picture.
Assume the reference GND plane is the 2nd layer and these trace parameters are for the Top layer only.

Can I verify my width and clearance values with your board house?
If the board house has a better number, I’d like to use that.


Hi, I was wondering if you plan on manufacturing stencils along with the PCB in the near future. Would love to try the service but ordering a separate stencil from another company adds delays and sometimes complication. Is it something you are working on or do you plan on producing only PCBs?

Stencils are definitely on the roadmap. :slight_smile:

I want to use the impedance calculator (Trace Impedance Calculator | DigiKey) to determine what my trace width should be, given that I’m using Digikey Red for my PCBs. For a microstrip trace type two parameters of interest are “trace thickness” and “height” - I’m presuming the latter is the height of the full PCB itself (or is it the layer?).

There are a few thickness values in this thread, but it isn’t clear to me which refer to layer thickness or trace thickness or pcb thickness, or something else entirely.

Does anyone have any tips for these things?

Hello,
check this link out DKRed | DigiKey for the different specifications for DK Red. On the board builder all of the attributes have a little “i” in a gray circle next to them. hover over the “i” and it will give you a description of what is needed. Thickness under the attributes is representing the board thickness.

Thanks for the response! In the calculator, I’m guessing the “height” parameter refers to the “thickness” parameter on the PCB builder, with the default being 1.5748 mm.

I’m guessing the “trace thickness” parameter refers to the “copper weight” parameter on the PCB builder, with the default being 1 oz.

Are these assumptions correct?

There’s also the dielectric constant - I’m not sure what that’s of (not copper I assume?) but other calculators seem to have a standard 4.3 for that value.