Hi
My board was working fine until yesterday.
After turning off my board yesterday, when I turned on the power again today, the following error message appeared.
U-Boot SPL 2019.01-dirty (Apr 14 2019 - 23:23:18 -0700)
Trying to boot from MMC2
Loading Environment from EXT4... Card did not respond to voltage select!
U-Boot 2019.01-dirty (Apr 14 2019 - 23:23:18 -0700)
CPU : AM335X-GP rev 2.1
I2C: ready
DRAM: 512 MiB
No match for driver 'omap_hsmmc'
No match for driver 'omap_hsmmc'
Some drivers were not found
Reset Source: Power-on reset has occurred.
RTC 32KCLK Source: External.
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Loading Environment from EXT4... Card did not respond to voltage select!
Board: BeagleBone Black
<ethaddr> not set. Validating first E-fuse MAC
BeagleBone Black:
Model: SeeedStudio BeagleBone Green:
BeagleBone: cape eeprom: i2c_probe: 0x54:
BeagleBone: cape eeprom: i2c_probe: 0x55:
BeagleBone: cape eeprom: i2c_probe: 0x56:
BeagleBone: cape eeprom: i2c_probe: 0x57:
Net: eth0: MII MODE
cpsw, usb_ether
Press SPACE to abort autoboot in 2 seconds
board_name=[BBG1] ...
Card did not respond to voltage select!
Card did not respond to voltage select!
Card did not respond to voltage select!
gpio: pin 56 (gpio 56) value is 0
gpio: pin 55 (gpio 55) value is 0
gpio: pin 54 (gpio 54) value is 0
gpio: pin 53 (gpio 53) value is 1
Card did not respond to voltage select!
Card did not respond to voltage select!
switch to partitions #0, OK
mmc1(part 0) is current device
Scanning mmc 1:1...
gpio: pin 56 (gpio 56) value is 0
gpio: pin 55 (gpio 55) value is 0
gpio: pin 54 (gpio 54) value is 0
gpio: pin 53 (gpio 53) value is 1
switch to partitions #0, OK
mmc1(part 0) is current device
gpio: pin 54 (gpio 54) value is 1
Checking for: /uEnv.txt ...
Checking for: /boot.scr ...
Checking for: /boot/boot.scr ...
Checking for: /boot/uEnv.txt ...
** Invalid partition 2 **
** Invalid partition 3 **
** Invalid partition 4 **
** Invalid partition 5 **
** Invalid partition 6 **
** Invalid partition 7 **
starting USB...
USB0: Port not available.
cpsw Waiting for PHY auto negotiation to complete......... TIMEOUT !
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC 60:64:05:46:64:08
HOST MAC de:ad:be:af:00:00
RNDIS ready
The remote end did not respond in time.missing environment variable: pxeuuid
Retrieving file: pxelinux.cfg/01-60-64-05-46-64-08
cpsw Waiting for PHY auto negotiation to complete......... TIMEOUT !
using musb-hdrc, OUT ep1out IN ep1in STATUS ep2in
MAC 60:64:05:46:64:08
HOST MAC de:ad:be:af:00:00
RNDIS ready
The message ‘RNDIS Ready’ appears repeatedly, and at the end, it goes to the Boot prompt.
There seems to be something wrong with my board, but I want to know when such error messages appear.
Could you let me know when the messages appear?
Please help me.
Regards.