I’m having an issue regarding my breakout board connected to a Raspberry pi 5. The issue I’m having is a no VoSPI detection. I’ve used a multimeter to test out the volts of each pin out. I found that pins; 8,9, 10,11,12,13,14 pinouts show no voltage. How can I fix this issue? The pin out that im specifically using are pins 1,2,5,7,8,9,10,12,15. Any advise or any answer would be appreciated. Thankyou.
Here is an older guide: Lepton/docs/RaspberryPiGuide.md at main · FLIR/Lepton · GitHub do you have spi overlay enabled?
Regards,
Yes, I do have it on, I’ve been trying many programs that tests the SPI ports of the breakout board it all seems to tell me that between the 3 pins of the breakout board v2 8 10 12 are faulty. This issue started after I fixed an issue regarding the I2C connectors which later was fixed.