Introduction
This page will show you step-by-step how to interface a FLIR Lepton module to the BeagleBone Black/Green.
Hardware Requirements
BeagleBone Black at DigiKey
BeagleBone Green at DigiKey
LCD4/LCD7 for BeagleBone Black/Green:
LCD4 at DigiKey
LCD7 at DigiKey
FLIR Lepton:
Lepton Breakout Board at DigiKey
FLIR CAMERA IR 80X60 50 DEGREE 9HZ at DigiKey
FLIR CAMERA IR 80X60 50 DEG W/SHUTTER at DigiKey
FLIR CAMERA IR 80X60 25 DEGREE 9HZ at DigiKey
Software Requirements
- BeagleBone Black/Green running Debian Stretch (iot image) flash to the eMMC
- Grab the Latest from: http://elinux.org/Beagleboard:BeagleBoneBlack_Debian#Stretch_IOT
Install latest console image to eMMC
Today the latest version is: 2018-10-07 ( these are just monthly snapshots, so always check for the latest )
IOT Image: (BeagleBone Black/Green eMMC)
wget https://rcn-ee.net/rootfs/bb.org/testing/2018-10-07/stretch-iot/BBB-blank-debian-9.5-iot-armhf-2018-10-07-4gb.img.xz
sha256sum: dcd36dcd330d2c6959f86ed13ce88c79515052dcd5c184dd75b0f19ec6c2be02
Insert microSD into pc adapter and check device node name (in our case /dev/sdd):
voodoo@hades:~$ lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT
sde 8:64 1 3.7G 0 disk
└─sde1 8:65 1 3.3G 0 part
sda 8:0 0 465.8G 0 disk
└─sda1 8:1 0 465.8G 0 part /
Download the *.img.xz and write to microSD card via etcher.io:
voodoo@hades:~$ wget https:` `//rcn-ee.net/rootfs/bb.org/testing/2018-10-07/stretch-iot/BBB-blank-debian-9.5-iot-armhf-2018-10-07-4gb.img.xz
voodoo@hades:~$ sudo /opt/etcher-cli/etcher -d /dev/sdf BBB-blank-debian-9.5-iot-armhf-2018-10-07-4gb.img.xz
? This will erase the selected drive. Are you sure? Yes
Flashing: 17.08 MB/s [========================] 100% eta 0s
Validating: 0 B/s [========================] 100% eta 0s
Checksums:
- /dev/sdf: d3aae7d1a808c4826f1e0b45d6d1bac3876ea55cacbb38225d5428d27f4e990ec25ad3e85bd503212a63da2e3fceda7cb666cb4977a02dbd94caf676c1d88cfd`
Insert microSD into BeagleBone Black/Green and wait for flashing procedure to finish. (device should shutdown)
Utilize g_serial on usb mini connector
Since we will be using an LCD, we will be losing access to the J1 serial debug header on the baseboard, you can use the pre-loaded g_serial module via: (note, no boot logs will be shown)
gtkterm -p /dev/ttyACM0 -s 115200 &
Setup basic window manager
For this project we are going to use openbox & slim to provide a very basic desktop environment on the LCD.
sudo apt update
sudo apt upgrade
sudo apt install openbox slim xinit xserver-xorg-video-fbdev x11-xserver-utils git libpam-gnome-keyring feh i2c-tools unclutter
Setup /etc/X11/xorg.conf
#/etc/X11/xorg.conf
Section "Monitor"
Identifier "Builtin Default Monitor"
EndSection
Section "Device"
Identifier "Builtin Default fbdev Device 0"
Driver "fbdev"
EndSection
Section "Screen"
Identifier "Builtin Default fbdev Screen 0"
Device "Builtin Default fbdev Device 0"
Monitor "Builtin Default Monitor"
EndSection
Section "ServerLayout"
Identifier "Builtin Default Layout"
Screen "Builtin Default fbdev Screen 0"
EndSection
Check bootloader version
debian@beaglebone:~$ sudo /opt/scripts/tools/version.sh | grep bootloader
bootloader:[eMMC-(default)]:[/dev/mmcblk1]:[U-Boot 2018.03-00002-gac9cce7c6a]:[location: dd MBR]
Update Kernel:
debian@beaglebone:~$ cd /opt/scripts/tools/
debian@beaglebone:/opt/scripts/tools$ sudo ./update_kernel.sh --lts-4_14
Install device tree overlays source for LCD4/LCD7
git clone https://github.com/beagleboard/bb.org-overlays --depth=1
cd ./bb.org-overlays
./dtc-overlay.sh
./install.sh
Shutdown system via:
sudo systemctl poweroff
Install LCD4/LCD7 and powerup BeagleBone Black/Green
Configure SLIM for autologin
Set Default User:
#/etc/slim.conf
# default user, leave blank or remove this line
# for avoid pre-loading the username.
#default_user simone
default_user debian
Enable auto-login
#/etc/slim.conf
# Automatically login the default user (without entering
# the password. Set to "yes" to enable this feature
#auto_login no
auto_login yes
Enable openbox:
echo "exec openbox-session" > /home/debian/.xsession
Lepton qt application
Build/Install Lepton application
sudo apt install build-essential qt4-dev-tools
git clone https://github.com/groupgets/LeptonModule
Apply this patch, to push the application to the upper left:
diff --git a/software/beagleboneblack_video/main.cpp b/software/beagleboneblack_video/main.cpp
index 264b0a2..f31c467 100644
--- a/software/beagleboneblack_video/main.cpp
+++ b/software/beagleboneblack_video/main.cpp
@@ -18,7 +18,7 @@ int main( int argc, char **argv )
QApplication a( argc, argv );
QWidget *myWidget = new QWidget;
- myWidget->setGeometry(400, 300, 340, 290);
+ myWidget->setGeometry(20, 20, 340, 290);
//create an image placeholder for myLabel
//fill the top left corner with red, just bcuz
and finally build the project
mkdir -p /home/debian/.config/openbox/
echo "feh --bg-scale /opt/scripts/images/beaglebg.jpg" > /home/debian/.config/openbox/autostart
echo "/home/debian/LeptonModule/software/beagleboneblack_video/bbb &" >> /home/debian/.config/openbox/autostart
Increase LCD brightness
echo "echo 100 >> /sys/devices/platform/backlight/backlight/backlight/brightness" >> /opt/scripts/boot/am335x_evm.sh
LCD4 Setup
Enable the “BB_SPIDEV0” overlay in /boot/uEnv.txt:
uboot_overlay_addr4=/lib/firmware/BB-SPIDEV0-00A0.dtbo
LCD7 Setup
We need P9.30 for SPIDEV1, which is the enter key on the LCD7, so disable P9.30 in BB-BONE-LCD7-01-00A3.dts
diff --git a/src/arm/BB-BONE-LCD7-01-00A3.dts b/src/arm/BB-BONE-LCD7-01-00A3.dts
index a1c7833..4fdfc2d 100644
--- a/src/arm/BB-BONE-LCD7-01-00A3.dts
+++ b/src/arm/BB-BONE-LCD7-01-00A3.dts
@@ -48,7 +48,6 @@
"P9.15", /* keys: gpio1_16 LEFT */
"P9.23", /* keys: gpio1_17 RIGHT */
"P9.16", /* keys: gpio1_19 UP */
- "P9.30", /* keys: gpio3_16 DOWN */
"P9.21", /* keys: gpio0_3 ENTER */
"ehrpwm1a",
@@ -57,7 +56,6 @@
"gpio1_16", /* LEFT */
"gpio1_17", /* RIGHT */
"gpio1_19", /* UP */
- "gpio3_16", /* DOWN */
"gpio0_3", /* ENTER */
"lcdc",
"tscadc";
@@ -111,7 +109,6 @@
BONE_P9_15 (PIN_INPUT | MUX_MODE7) /* gpmc_a0.gpio1_16 */
BONE_P9_23 (PIN_INPUT | MUX_MODE7) /* gpmc_a1.gpio1_17 */
BONE_P9_16 (PIN_INPUT | MUX_MODE7) /* gpmc_a3.gpio1_19 */
- BONE_P9_30 (PIN_INPUT | MUX_MODE7) /* mcasp0_axr0.gpio3_16 */
BONE_P9_21 (PIN_INPUT | MUX_MODE7) /* spi0_d0.gpio0_3 */
>;
};
@@ -222,14 +219,6 @@
};
button@4 {
debounce_interval = <50>;
- linux,code = <108>;
- label = "down";
- gpios = <&gpio3 16 0x1>;
- gpio-key,wakeup;
- autorepeat;
- };
- button@5 {
- debounce_interval = <50>;
linux,code = <28>;
label = "enter";
gpios = <&gpio0 3 0x1>;
Then rebuild:
cd ./bb.org-overlays
make clean
./install.sh
Enable the “BB_SPIDEV1” overlay in /boot/uEnv.txt:
uboot_overlay_addr4=/lib/firmware/BB-SPIDEV1-00A0.dtbo
Comments
Any questions or comments please go to our TechForum: TechForum