Created by Robert Nelson, last modified on Jan 25, 2016
Introduction
This page will show you step-by-step how to interface a NimbeLink cape to the BeagleBone Black/Green.
Hardware Requirements
BeagleBone Black at DigiKey
BeagleBone Green at DigiKey
NimbeLink Beaglebone Black IOT cape:
NL-AB-BBBC at DigiKey
XBee XB24CZ7WIT-004 at DigiKey
Software Requirements
- BeagleBone Black/Green running Debian Jessie (console image) flash to the eMMC
- Grab the Latest from: Making sure you're not a bot!
Install latest console image to eMMC
Today the latest version is: 2016-01-03 ( these are just weekly snapshots, so always check for the latest )
Flasher: (console) (BeagleBone Black/Green eMMC)
wget https://rcn-ee.com/rootfs/bb.org/testing/2016-01-03/console/BBB-eMMC-flasher-debian-8.2-console-armhf-2016-01-03-2gb.img.xz
sha256sum: ecd682d199d98abbff46e187cd1ccb51e9776645a5aa28f35d0d5e9c92127ec4
Insert microSD into pc adapter and check device node name (in our case /dev/sdd):
voodoo@hades:~$ lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT
sda 8:0 0 465.8G 0 disk
└─sda1 8:1 0 465.8G 0 part /
sdd 8:48 1 7.4G 0 disk
└─sdd1 8:49 1 7.4G 0 part
Download the *.img.xz and matching *.bmap file, and write to microSD card via bmaptools:
voodoo@hades:~$ wget https://rcn-ee.com/rootfs/bb.org/testing/2016-01-03/console/BBB-eMMC-flasher-debian-8.2-console-armhf-2016-01-03-2gb.img.xz
voodoo@hades:~$ wget https://rcn-ee.com/rootfs/bb.org/testing/2016-01-03/console/BBB-eMMC-flasher-debian-8.2-console-armhf-2016-01-03-2gb.bmap
voodoo@hades:~$ sudo bmaptool copy --bmap BBB-eMMC-flasher-debian-8.2-console-armhf-2016-01-03-2gb.bmap BBB-eMMC-flasher-debian-8.2-console-armhf-2016-01-03-2gb.img.xz /dev/sdd
[sudo] password for voodoo:
bmaptool: info: block map format version 2.0
bmaptool: info: 435200 blocks of size 4096 (1.7 GiB), mapped 79584 blocks (310.9 MiB or 18.3%)
bmaptool: info: copying image 'BBB-eMMC-flasher-debian-8.2-console-armhf-2016-01-03-2gb.img.xz' to block device '/dev/sdd' using bmap file 'BBB-eMMC-flasher-debian-8.2-console-armhf-2016-01-03-2gb.bmap'
bmaptool: info: 100% copied
bmaptool: info: synchronizing '/dev/sdd'
bmaptool: info: copying time: 1m 20.9s, copying speed 3.8 MiB/sec
Insert microSD into the first BeagleBone Black/Green and wait for flashing procedure to finish. (device should shutdown)
Enable g_serial on usb mini connector
Since we will be using an NimbeLink cape, we will be losing access to the J1 serial debug header on the baseboard. So let’s enable “g_serial” over the usb mini by default. We can have current am335x_evm boot script to this for us, by removing “udhcpd”
#If image file is found, use it for g_multi
if [ -f ${usb_image_file} ] ; then
modprobe g_multi file=${usb_image_file} cdrom=0 ro=0 stall=0 removable=1 nofua=1 ${g_network} || true
#In a single partition setup, dont load g_multi, as we could trash the linux file system...
elif [ "x${root_drive}" = "x/dev/mmcblk0p1" ] || [ "x${root_drive}" = "x/dev/mmcblk1p1" ] ; then
if [ -f /usr/sbin/udhcpd ] || [ -f /usr/sbin/dnsmasq ] ; then
#Make sure (# CONFIG_USB_ETH_EEM is not set), otherwise this shows up as "usb0" instead of ethX on host pc..
modprobe g_ether ${g_network} || true
else
#serial:
modprobe g_serial || true
fi
else
boot_drive="${root_drive%?}1"
modprobe g_multi file=${boot_drive} cdrom=0 ro=0 stall=0 removable=1 nofua=1 ${g_network} || true
fi
Let’s remove udhcpd
debian@beaglebone:~$ sudo apt-get remove udhcpd --purge
Reading package lists... Done
Building dependency tree
Reading state information... Done
The following packages will be REMOVED:
udhcpd*
0 upgraded, 0 newly installed, 1 to remove and 0 not upgraded.
After this operation, 88.1 kB disk space will be freed.
Do you want to continue? [Y/n] y
(Reading database ... 12104 files and directories currently installed.)
Removing udhcpd (1:1.22.0-9+deb8u1) ...
Purging configuration files for udhcpd (1:1.22.0-9+deb8u1) ...
On the next reboot:
[13188.095975] usb 5-1.4: new high-speed USB device number 5 using xhci_hcd
[13188.186421] usb 5-1.4: New USB device found, idVendor=0525, idProduct=a4a7
[13188.186426] usb 5-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[13188.186428] usb 5-1.4: Product: Gadget Serial v2.4
[13188.186430] usb 5-1.4: Manufacturer: Linux 4.1.13-ti-r34 with musb-hdrc
[13188.200414] cdc_acm 5-1.4:2.0: ttyACM0: USB ACM device
[13188.200922] usbcore: registered new interface driver cdc_acm
[13188.200925] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
Using gtkterm we can get access via:
gtkterm -p /dev/ttyACM0 -s 115200 &
Install common tools
For this project we are going to use just a few tools on top of the base console image.
sudo apt-get update
sudo apt-get install bc git-core i2c-tools picocom ppp python-dev python-setuptools usbutils
Update /boot/uEnv.txt to use the correct dtb for NimbeLink and eMMC usage
sudo sed -i 's/#dtb=$/dtb=am335x-boneblack-emmc-overlay.dtb/' /boot/uEnv.txt
Install device tree overlays for NimbeLink cape
git clone https://github.com/beagleboard/bb.org-overlays --depth=1
cd ./bb.org-overlays
./dtc-overlay.sh
./install.sh
cd ~/
Update Kernel (the 2016-01-03 default kernel lacks the driver for the iio based temp sensor we are using in this example.)
cd /opt/scripts/tools/
git pull
sudo ./update_kernel.sh --ti-rt-channel --lts-4_1
cd ~/
Install Exoline
git clone https://github.com/exosite/exoline --depth=1
cd ./exoline
sudo python setup.py install
cd ~/
Disable eth0
sudo sed -i 's/auto eth0$/#auto eth0/' /etc/network/interfaces
sudo sed -i 's/iface eth0 inet dhcp$/#iface eth0 inet dhcp/' /etc/network/interfaces
Cleanup and Shutdown system via:
sudo apt-get clean
sudo systemctl poweroff
Install NimbeLink and powerup BeagleBone Black/Green and verify cape is installed, since j1 debug is hidden use the usb port:
gtkterm -p /dev/ttyACM0 -s 115200 &
debian@beaglebone:~$ dmesg | grep bone
[ 3.976746] bone_capemgr bone_capemgr: Baseboard: 'A335BNLT,,BBG115091797'
[ 3.976783] bone_capemgr bone_capemgr: compatible-baseboard=ti,beaglebone-black - #slots=4
[ 4.032343] bone_capemgr bone_capemgr: slot #0: No cape found
[ 4.092306] bone_capemgr bone_capemgr: slot #1: No cape found
[ 4.152301] bone_capemgr bone_capemgr: slot #2: No cape found
[ 4.182329] bone_capemgr bone_capemgr: slot #3: 'Skywire Beaglebone Cape,00D0,Nimbelink,NL-AB-BBBC'
[ 4.182849] bone_capemgr bone_capemgr: initialized OK.
[ 4.211219] bone_capemgr bone_capemgr: slot #3: dtbo 'NL-AB-BBBC-00D0.dtbo' loaded; overlay id #0
debian@beaglebone:~$ cat /sys/devices/platform/bone_capemgr/slots
0: PF---- -1
1: PF---- -1
2: PF---- -1
3: P---L- 0 Skywire Beaglebone Cape,00D0,Nimbelink,NL-AB-BBBC
Clone eMMC
Insert a microSD into BeagleBone Black/Green that we will use to clone the eMMC to the additional device.
debian@beaglebone:~$ lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT
mmcblk0boot0 179:8 0 2M 1 disk
mmcblk0boot1 179:16 0 2M 1 disk
mmcblk0 179:0 0 3.6G 0 disk
`-mmcblk0p1 179:1 0 3.6G 0 part /
mmcblk1 179:24 0 3.7G 0 disk <<< Inserted microSD >>>
`-mmcblk1p1 179:25 0 1.7G 0 part
Run “beaglebone-black-make-microSD-flasher-from-eMMC.sh” script
cd /opt/scripts/tools/eMMC
sudo ./beaglebone-black-make-microSD-flasher-from-eMMC.sh
Progress:
-----------------------------
Version: [1.20151007: gpt partitions with raw boot...]
-----------------------------
copying: [/dev/mmcblk0] -> [/dev/mmcblk1]
lsblk:
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT
mmcblk0boot0 179:8 0 2M 1 disk
mmcblk0boot1 179:16 0 2M 1 disk
mmcblk0 179:0 0 3.6G 0 disk
`-mmcblk0p1 179:1 0 3.6G 0 part /
mmcblk1 179:24 0 3.7G 0 disk
`-mmcblk1p1 179:25 0 1.7G 0 part
-----------------------------
df -h | grep rootfs:
-----------------------------
update-initramfs: Generating /boot/initrd.img-4.1.13-ti-rt-r39
<<< RUNNING >>>
Shutdown system via:
sudo systemctl poweroff
Remove “microSD” and flash other BeagleBone Black/Green devices.
XBee Setup
Download and install XCTU: Digi XCTU — Download and Install the Configuration Platform for XBee/RF Solutions | Digi International
Gateway Xbee: (13A200 40F536D8)
PAN ID: 4113
Coordinator Enable: Enabled [1]
Sensor Xbee: (13A200 40E5F1AD)
PAN ID: 4113
Destination Address High: 13A200
Destination Address Low: 40F536D8
Test, with both Xbee’s installed in their ownNimbeLink cape:
echo "test" > /dev/ttyS2
Temperature Sensor
Add device:
sudo sh -c "echo si7005 0x40 > /sys/bus/i2c/devices/i2c-2/new_device"
debian@beaglebone:~$ dmesg | grep i2c-2
[ 228.452700] i2c i2c-2: new_device: Instantiated device si7005 at 0x40
Look at the device:
debian@beaglebone:~$ ls /sys/bus/iio/devices/iio\:device0/in_temp*
/sys/bus/iio/devices/iio:device0/in_temp_offset
/sys/bus/iio/devices/iio:device0/in_temp_raw
/sys/bus/iio/devices/iio:device0/in_temp_scale
debian@beaglebone:~$ cat /sys/bus/iio/devices/iio:device0/in_temp*
-6400
9704
7.812500
Conversion:
T = ((in_temp0_raw + in_temp0_offset) * in_temp0_scale) / 1000
T = ((9704 + -6400) * 7.812500) / 1000
T = (3304 * 7.812500) / 1000
T = 25812.5 / 1000
T = 25.8125 (C) 78.4625 (F)
Script the conversion using bc:
#!/bin/bash -e
in_temp_raw=$(cat /sys/bus/iio/devices/iio:device0/in_temp_raw || true)
in_temp_offset=$(cat /sys/bus/iio/devices/iio:device0/in_temp_offset || true)
in_temp_scale=$(cat /sys/bus/iio/devices/iio:device0/in_temp_scale || true)
if [ ! "x${in_temp_raw}" = "x" ] && [ ! "x${in_temp_offset}" = "x" ] && [ ! "x${in_temp_scale}" = "x" ] ; then
temp=$(echo "${in_temp_raw} + ${in_temp_offset}" | bc)
temp=$(echo "scale=5; ${temp} * ${in_temp_scale}" | bc)
temp=$(echo "scale=5; ${temp} / 1000" | bc)
echo "${temp}"
fi
Now send that data padded with a cksum over the serial port:
#!/bin/bash -e
port="/dev/ttyS2"
send_data () {
date_cksum=$(echo ${data} | cksum | awk '{print $1}')
echo "\$${data}*${date_cksum}#"
echo -e "\$${data}*${date_cksum}#\n" > ${port}
}
stty -F ${port} raw speed 9600 &> /dev/null
in_temp_raw=$(cat /sys/bus/iio/devices/iio:device0/in_temp_raw || true)
in_temp_offset=$(cat /sys/bus/iio/devices/iio:device0/in_temp_offset || true)
in_temp_scale=$(cat /sys/bus/iio/devices/iio:device0/in_temp_scale || true)
if [ ! "x${in_temp_raw}" = "x" ] && [ ! "x${in_temp_offset}" = "x" ] && [ ! "x${in_temp_scale}" = "x" ] ; then
temp=$(echo "${in_temp_raw} + ${in_temp_offset}" | bc)
temp=$(echo "scale=5; ${temp} * ${in_temp_scale}" | bc)
temp=$(echo "scale=5; ${temp} / 1000" | bc)
data="TEXT,TEMP0,${temp},"
send_data
fi
and load the iio driver if not loaded (assumes root)
#!/bin/bash -e
port="/dev/ttyS2"
send_data () {
date_cksum=$(echo ${data} | cksum | awk '{print $1}')
echo "\$${data}*${date_cksum}#"
echo -e "\$${data}*${date_cksum}#\n" > ${port}
}
stty -F ${port} raw speed 9600 &> /dev/null
if [ ! -f /sys/bus/iio/devices/iio:device0/in_temp_raw ] ; then
echo si7005 0x40 > /sys/bus/i2c/devices/i2c-2/new_device
fi
in_temp_raw=$(cat /sys/bus/iio/devices/iio:device0/in_temp_raw || true)
in_temp_offset=$(cat /sys/bus/iio/devices/iio:device0/in_temp_offset || true)
in_temp_scale=$(cat /sys/bus/iio/devices/iio:device0/in_temp_scale || true)
if [ ! "x${in_temp_raw}" = "x" ] && [ ! "x${in_temp_offset}" = "x" ] && [ ! "x${in_temp_scale}" = "x" ] ; then
temp=$(echo "${in_temp_raw} + ${in_temp_offset}" | bc)
temp=$(echo "scale=5; ${temp} * ${in_temp_scale}" | bc)
temp=$(echo "scale=5; ${temp} / 1000" | bc)
data="TEXT,TEMP0,${temp},"
send_data
fi
tie into cron
/etc/crontab
# m h dom mon dow user command
17 * * * * root cd / && run-parts --report /etc/cron.hourly
25 6 * * * root test -x /usr/sbin/anacron || ( cd / && run-parts --report /etc/cron.daily )
47 6 * * 7 root test -x /usr/sbin/anacron || ( cd / && run-parts --report /etc/cron.weekly )
52 6 1 * * root test -x /usr/sbin/anacron || ( cd / && run-parts --report /etc/cron.monthly )
* * * * * root /bin/bash /home/debian/tx_temp.sh &> /dev/null &
#
Receiver
We need P9.30 for SPIDEV1, which is the enter key on the LCD7, so disable P9.30 in BB-BONE-LCD7-01-00A3.dts