Get Started Quickly with the PIC-IoT WA Development Board – Online Programming Guide

PIC-IoT WA Development Board ( EV54Y39A) integrates an all-in-one on-board debugger, eliminating the need for an external programmer. Online programming and debugging can be accomplished solely via a USB cable. This built-in debugger supports drag-and-drop programming, virtual serial port communication, and debugging within MPLAB X IDE, greatly streamlining the development workflow.

Core Hardware & Interfaces

The integrated composite USB debugger incorporates four key functions:

  1. MPLAB X IDE Debugger: Enables firmware programming and in-circuit debugging for the PIC24FJ128GA705 MCU.
  2. Mass Storage Device: Supports drag-and-drop programming; simply copy the compiled .hex firmware file to the board’s drive letter to complete flashing.
  3. CDC Virtual Serial Port: Interfaces with the on-board hardware UART to output application logs and support bidirectional interaction via terminal software.
  4. Data Gateway Interface (DGI): Works with a logic analyzer to deliver visual program flow debugging.

Key Status Indications via PS LED

Operating Mode LED Status Description
Power-up / Normal Operation Steady ON
Successful Drag-and-Drop Programming Slow blink (~1 Hz) for 2 seconds
Failed Drag-and-Drop Programming / Power Supply Fault Fast blink (~5 Hz) for 2 seconds
Firmware Flashing / Active Debugging Continuous slow blink (~1 Hz)
External Power Supply / Sleep Mode LED OFF

Key Operation Steps

  1. Connect the USB cable to your PC and wait for the debugger to finish enumeration (PS LED lights up steadily).
  2. Drag-and-Drop Programming: Copy the compiled .hex file to the debugger’s virtual mass storage drive, and check the LED blink pattern to verify the flashing result.
  3. IDE Debugging: Select the on-board debugger inside MPLAB X IDE to perform one-click firmware download and in-circuit debugging.
  4. Serial Port Interaction: After the PC recognizes the virtual COM port, configure the matching baud rate in terminal software (e.g., TeraTerm) to view real-time application logs.


(Images sourced from Microchip)

CDC (Communications Device Class) Virtual Serial Port of the On-Board Debugger on PIC-IoT WA Development Board

Tech Tip :The slow blink rate is roughly 1 Hz, and the fast blink rate is approximately 5 Hz. You can rapidly diagnose issues using the LED blink frequency. For example, if programming fails, first verify the integrity of the firmware file and the stability of the USB connection.

Related Documents

Related Products

  • PIC-IoT WA Development Board ( EV54Y39A)

Related Articles

  1. Get Started Quickly with the PIC-IoT WA Development Board – A Quick Start Guide
  2. Get Started Quickly with the PIC-IoT WA Development Board – On-Board Resource Breakdown
  3. Get Started Quickly with the PIC-IoT WA Development Board – Power Supply Configuration Guide
  4. Get Started Quickly with the PIC-IoT WA Development Board – Online Programming Guide
  5. Get Started Quickly with the PIC-IoT WA Development Board – CDC Virtual Serial Port