Help Finding Twisted Pair Wire PN

Hello,

Can someone help me find a suitable DigiKey part number for the following application? There are so many part numbers and most of them seem to come in giant spools of 1000 ft.

Looking for a 30-50 ft length of 20 ga twisted pair (single pair - 2 conductors) stranded copper wiring suitable for CANbus communication in an automobile.

The application is to run these wires from the car’s ECU in the trunk to some gauges in the cabin (VADpro 15). I’d like it to have some insulation to protect it from the elements.

If someone could recommend me a part number that would be awesome!!! Thank you!

Hello,

Take a look at the part number in this link.

Thanks Karl! That’s a big help.

I’m leaning towards the 1033A 01010000.

Just got a question about that one though. It looks like there is a smaller third wire. I think it’s called the drain wire? What does that do exactly? Is it just a ground wire? Would I attach it to the vehicle frame or just leave it unconnected?

Greetings,

It is not an equipment grounding conductor and should not be used as such, it isn’t designed to handle that much electricity. It is connected to the shielding of the wire and with the shielding forms a Faraday cage. The drain wire transfers small electrical impulses and unwanted electrical noise away from the main wires of the cable. It should be grounded on one end.

1 Like

Hi @Karl_1696 and @shawn_adams. Thanks for recommending me the cable. I appreciate the part number and information. I ended up ordering the IGUS CF891-05-02 and it works perfectly! Appreciate the support!