Help identifying diotec component

Hello,

I’m desperately trying to get help identifying a diotec component. At first I thought it was their M6 series diode however the component package I have is much larger than the M6 series. The component is roughly 5.5mm wide and 6.5mm long while being very thin at about 1.5mm thick.

The only markings on it are 33A and M*M6. I’m assuming 33A is the amp rating? I’ve tried cross referencing on the diotec site with no luck.

Hello SMPC88,
Thank you for posting on our forum and welcome to our community.
I think it might be one of the TVS diodes. I am to inform you that I am not able to filter sizes.