Help to identify sensor/accelerometer

Can anyone identify this silver vibration sensor/accelerometer used on these samples ? It runs on 4.5v batteries, is approximately 2.8mm x 1.8mm x 0.5mm, is used in very cheap toys to detect impact, and then have the IC turn on the LED lights for a few seconds.

Maybe the silver part is not an accelerometer. Very likely a metal-cased tilt or vibration switch. Something like the SW-18010P. These are much cheaper than accelerometers. MEMS accelerometers usually look like this.LSM6DSL iNEMO Inertial Module, Always-on 3D Accelerometer, and 3D Gyroscope - The Engineering Projects

Thank you very much for this reply. Certainly similar functionality, ultralow power consumption, low price, and similar footprint. Cannot tell how sensitive the LSM6DSL is though… like an SW-18010P, or more like SW-18030P Slow (less sensitive) ? Looking for a low sensitivity solution (needs to be struck to activate).

If you’re just after strike-to-activate behavior, want ultra-low complexity and price, and are okay with mechanical solutions, then SW-18030P is the easiest and most robust.

Hello @danoblenis

Welcome to the TechForum

Would you be able to get closer pictures of the chips that you are looking at?

Yes, attached are several close-ups of the component. No markings visible - may not be on the market. We did get one off the board, wired up, and captured trigger event on oscilloscope. Likely Piezoelectric, as high G shaking does not activate, tapping does. Finding a an ultra-low power component on the market with same/very similar sensitivity and form factor is the goal. Images: Top, Bottom, Side1.




END

Hello again danoblenis,
Thank you for contacting DigiKey Technical support.
I am sorry to inform you that I was not able to ID that part.