We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
I received a Hockey Puck SCR part # VS-ST230C12C0GI-ND.
When I Measured the Continuity between the Cathode and the Gate, it is a dead short, “Buzzes”
Is this Normal for a uninstalled Part…? Does the part need to be clamped down in the installation for it to not Buzz between the Cathode and the Gate…? Or is the part Bad…?
My 10A TO220 SCR parts do not Buzz between the Cathode and the Gate.
Welcome.
You may be biasing the internal diode. What number is reading on your meter when you are measuring continuity? You could try measuring across it with the meter in lowest resistance setting and see if that renders any values.
Ok, it has High resistance between the Cathode and the Anode in both directions. Also High resistance between between the Anode and the Gate in both directions.
Ok, so you think this is a good part…? Will clamping it down in the instillation change this behavior?
It is a spring loaded part, and Clamping it between 2 heat sinks with x amount of torque, is the installation.
The previous part with the same Part#, would show 11V on the gate when when installed, I thought I Had blown it up somehow… The very first part 238-N0465WN140-ND never showed 11V on the gate when installed. Unfortunately I killed it…
I guess what you are seeing is normal. The Thyristor is a 410A device, so expect to have quite a low resistance at the Gate. It needs 1.8V and 90mA at the gate to turn on. On datasheet page6 you can see from the curve in Fig. 11 that, for example, at 0.25Vgk the current Igk is 10mA, i.e. the resistance is 25 ohms.
However, the spec does not mention about the reverse gate biasing, thus cannot say if it is OK that the readings are same with both polarities (would imagine that there is a reverse protecting diode between gate and kathode, in which case it would explain the readings).