Below document describes: How to Enter and Use Command Mode to configure the sensor:
Command Mode HumidIcon TN_009062-3-EN_Final_07Jun12.pdf (207.9 KB)
Command Mode is used on the Honeywell HumidIcon™ Digital Humidity/Temperature Sensors for reading and writing to the on-chip EEPROM. Command Mode allows the user to configure and optimize sensor performance to match application requirements.
User-configurable options include alarm settings such as to send signal when humidity/temperature goes above and/or below user-programmed values, I2C address change which would allow more than one sensor to be connected on the same I2C bus, and customer identification bytes. The trick is that it would have to be configured for a different address before it is connected into the final system, such as during the production process.
See also:
Digi-Key I²C & SPI HumidIcon™ Sensor Selection
Honeywell HumidIcon™ 20, 21, 30, 31 Suffix Meaning
How to connect Honeywell CSNK500M Current Sensors
Honeywell HumidIcon™ HIH-8000 Sensor Handling Guidelines
Summary
480-6987-ND
480-5706-2-ND,480-5706-1-ND
HIH7120-021-001TR-ND,HIH7120-021-001CT-ND
480-5580-2-ND,480-5580-1-ND
480-3651-2-ND,480-3651-1-ND,480-3651-6-ND
480-6986-ND
480-5704-2-ND,480-5704-1-ND,480-5704-6-ND
480-3652-2-ND,480-3652-1-ND,480-3652-6-ND
480-6383-2-ND,480-6383-1-ND,480-6383-6-ND
HIH7130-000-001TR-ND,HIH7130-000-001CT-ND
480-5705-2-ND,480-5705-1-ND,480-5705-6-ND
2266-HIH7121-021-001S-ND,HIH7121-021-001S-ND
2266-HIH6031-000-001S-ND,HIH6031-000-001S-ND
2266-HIH6130-021-001S-ND,480-6684-ND
HIH8121-021-001S-ND
480-5581-2-ND,480-5581-1-ND
HIH9120-021-001TR-ND,HIH9120-021-001CT-ND,2266-HIH9120-021-001-ND
2266-HIH9130-021-001S-ND,HIH9130-021-001S-ND
2266-HIH8120-021-001S-ND,HIH8120-021-001S-ND
480-6773-ND
HIH7120-021-001S-ND
HIH9130-000-001S-ND
480-5909-ND
HIH6031-021-001S-ND
HIH8130-021-001TR-ND,HIH8130-021-001CT-ND,HIH8130-021-001DKR-ND
HIH8121-021-001TR-ND,HIH8121-021-001CT-ND
HIH8131-000-001S-ND
480-6382-2-ND,480-6382-1-ND,480-6382-6-ND
HIH8130-000-001S-ND
HIH8130-021-001S-ND
HIH6030-000-001S-ND
HIH7130-021-001S-ND
HIH6020-021-001TR-ND,HIH6020-021-001CT-ND
HIH9131-021-001TR-ND,HIH9131-021-001CT-ND,HIH9131-021-001DKR-ND
HIH6030-000-001TR-ND,HIH6030-000-001CT-ND,HIH6030-000-001DKR-ND
HIH6031-000-001TR-ND,HIH6031-000-001CT-ND,HIH6031-000-001DKR-ND
HIH8130-000-001TR-ND,HIH8130-000-001CT-ND,HIH8130-000-001DKR-ND
HIH8131-000-001TR-ND,HIH8131-000-001CT-ND,HIH8131-000-001DKR-ND
HIH7130-021-001TR-ND,HIH7130-021-001CT-ND
2266-HIH6131-021-001S-ND,480-6685-ND
HIH9120-021-001S-ND
HIH6031-021-001TR-ND,HIH6031-021-001CT-ND,HIH6031-021-001DKR-ND
HIH6021-021-001TR-ND,HIH6021-021-001CT-ND
HIH7131-021-001TR-ND,HIH7131-021-001CT-ND,HIH7131-021-001DKR-ND
HIH9121-021-001TR-ND,HIH9121-021-001CT-ND
HIH7121-021-001TR-ND,HIH7121-021-001CT-ND
480-5707-2-ND,480-5707-1-ND,480-5707-6-ND
HIH9130-000-001TR-ND,HIH9130-000-001CT-ND,HIH9130-000-001DKR-ND
2266-HIH7130-000-001S-ND,HIH7130-000-001S-ND
HIH7131-021-001S-ND
HIH6020-021-001S-ND
HIH8131-021-001TR-ND,HIH8131-021-001CT-ND,HIH8131-021-001DKR-ND
HIH9130-021-001TR-ND,HIH9130-021-001CT-ND,HIH9130-021-001DKR-ND
HIH9131-000-001S-ND
HIH8131-021-001S
HIH8120-021-001
HIH7120-021-001
HIH6121-021-001
HIH6130-021-001
HIH6021-021-001S
HIH6030-021-001
HIH6131-021-001
HIH6131-000-001
HIH7130-000-001
HIH7131-000-001
HIH7121-021-001S
HIH6031-000-001S
HIH6130-021-001S
HIH8121-021-001S
HIH6120-021-001
HIH9120-021-001
HIH9130-021-001S
HIH8120-021-001S
HIH9121-021-001S
HIH7120-021-001S
HIH9130-000-001S
HIH9131-021-001S
HIH6031-021-001S
HIH8130-021-001
HIH8121-021-001
HIH8131-000-001S
HIH6130-000-001
HIH8130-000-001S
HIH8130-021-001S
HIH6030-000-001S
HIH7130-021-001S
HIH6020-021-001
HIH9131-021-001
HIH6030-000-001
HIH6031-000-001
HIH8130-000-001
HIH8131-000-001
HIH7130-021-001
HIH6131-021-001S
HIH9120-021-001S
HIH6031-021-001
HIH6021-021-001
HIH7131-021-001
HIH9121-021-001
HIH7121-021-001
HIH9131-000-001
HIH9130-000-001
HIH7130-000-001S
HIH7131-021-001S
HIH6020-021-001S
HIH8131-021-001
HIH9130-021-001
HIH9131-000-001S