We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
What do I need to integrate a charge controller at 12VDC hooked up to PV & battery with a power supply getting 120VAC? I have loads at 12VDC and 5VDC. The power supply has dual output for 5VDC and 12VDC, so I can use that when the battery is low. But then I want the PV and/or power supply to charge the battery and if power supply is unplugged, it can run off the battery.
I’m working on a block diagram and what I need in which state etc, but I’m wondering what is normally used for applications like this. Is there a specific product that I should be aware of before I start building something and hooking things up strangely?
The ‘GND bus’ shown is also connected to all other GND symbols shown on the sketch, apologize for the confusion having separate symbols. I have not connected the +/- LOAD terminals as shown.
I assume would it have to come from a switched output. So the charge ctrlr would be 1 input and 2nd is power supply, and 1 output is either 12V from pwr supply or charge ctrlr based on if pwr supply is on or not. Correct?
I’m starting to think I need to use a different charge controller which accepts 120VAC, and just do the 12V to 5V conversion with an external piece. Does anyone know of a charge controller that would take the 120VAC and use it to charge the battery in the case that it’s present & solar output is not, and offer 12V output?