Question:
How do I open and close DC using a basic switch?
![]()
Answer:
In direct current switching, the arc (spark generated between the contacts upon switching) lasts longer, causing more severe contact wear compared to alternating current. When cutting off a DC circuit, please select a switch with a DC rating and use it according to the rating.
![]()
Explanation:
In an AC circuit in which the direction of current flow changes, the arc disappears each time the voltage becomes overvoltage (OV). But in a DC circuit, the direction of flow remains unchanged, which increases the duration of the arc, causing contact wear and less durability.
In addition, the transfer phenomenon of the contact may occur, which may cause unevenness in the contact and a malfunction that prevents the contact from being opened.
![]()
Quick tips
Please consider X series: Direct-current basic switch with built-in magnetic blow-out, if the size of X is acceptable.
Product category
Switches Basic Switches
Classification
Usage, Applications
Related keywords
Basic Switch
Direct Current
DC Switching
Arc
![]()
Please visit the link below to see this product category on the Digi-Key website
Switches | DigiKey Electronics
This FAQ has been brought to you courtesy of
Please click the link below to view the original FAQ