The nRF9160 Feather IoT Development Board is a powerful and compact device that can be used for developing IoT applications that use cellular networks. These are the steps needed to turn up the board and get it connected to a cellular network.
-
Assemble the hardware - To start, you will need to assemble the hardware. This involves connecting the antenna to the board, inserting a SIM card into the slot, and connecting any other peripherals you may need.
-
Install the necessary software - Next, you will need to install the software necessary to communicate with the board. This includes the Nordic Semiconductor nRF Connect for Desktop software and the necessary device drivers. Or visit Jared Wolffโs site for more information.
-
Insert the SIM and configure the board - Insert a valid and activated SIM card into the boardโs SIM slot. The SIM card should support NBIoT or Cat-M network technology. Once the SIM and software is installed, you will need to configure the board. This involves setting up the cellular network settings, such as the APN, username, and password. Soracom IoT connectivity options.
-
Test the connection - After configuring the board, you can now test the connection. This can be done using the nRF Connect for Desktop software by sending AT commands to the board.
-
Develop your application - With the board connected to the cellular network, you can now start developing your IoT application. This simple guide from Jared Wolff on his nRF9160 feather board is a great place to start. The software development kits, code and examples have links to the various operating systems, Windows, MacOS and Linuxโฆ
-
Deploy and monitor your application - Finally, once your application is developed, you can deploy it to the board and monitor it to ensure it is functioning correctly. This can be done using the nRF Connect for Desktop software, as well as any other monitoring tools you may need.
Turning up an nRF9160 Feather IoT Development Board on a cellular network is a simple process that can be completed by following these steps. With this powerful and compact device, you can easily develop and deploy IoT applications that use cellular networks.