Click Image to Enlarge:
Topping charge, sometimes called trickle or float charge, is applied on a battery that is in service or storage to maintain full charge and to prevent sulfation on lead acid batteries.
CAUTION: Under no circumstances should batteries be incinerated, as fire can cause an explosion. Wear approved gloves when touching electrolyte. On exposure to skin, flush with water immediately. If eye exposure occurs, flush with water for 15 minutes and consult a physician immediately. Overcharging of batteries can cause fire, explosion, chemical spill and/or poisonous chemical gas.
See Also:
Charging Lead Acid Battery Basics
Reference:
https://www.zeusbatteryproducts.com/wp-content/uploads/2020/11/Summary-of-Dos-and-Donts.pdf
We now have a product that will take care of battery recycling for you. Battery Solutions iRecycle Kit 55 (part # 4280-RKP3W55-ND), is a complete recycling kit offering not only the container, but also includes pre-paid recycling and return shipping costs. This is perfect for businesses and schools who need a recycling solution for batteries.
After ordering, you will receive a UN approved collection pail capable of holding 55 pounds of various batteries. Simply add the batteries to the pail, and once it reaches capacity you send it back to the supplier and they will take care of the recycling process.
This pail works with numerous battery technologies including Alkaline, NiCd, NiMH, Lithium Ion, Silver Oxide, Button Cells, Mercury, Lead Acid and more. You can even put small electronics such as cellphones, activity trackers, smart watches, earbuds, etc) into the bucket for recycling too.

1 Like
GlobTek provides detailed use and charging instructions on it’s website for it’s Lithium Ion battery packs, many of which are IEC62133 certified and in stock @ Digikey: