Can someone help me identify these components and their correct replacement part numbers please?
See pics
Hello,
Welcome to the Digikey forum. Do you have any information listing the values of these parts? Are you referring to all of them or just a few? Any information you can provide on part descriptions would be helpful.
I’m partially color blind but I’ll send a closeup pic along with what I can make out with my old eyes.
C20 and C14
XL3 9513
—————
D3
Maybe 166
——————
R8
Orange white gray?
—————————
Z1
Black cover silver band at one end.
Has a Y marking.
————————-
R9 Green Red Orange. I’m in real question about these colors.
I’m going to attach some more pics of front and back and a detailed pic so maybe you can tell what they are.
Also if you think any of the other components on the board may also be in question I’ll be glad to provide you with detailed pics. Just let me know what location numbers.
Thank you so much for any help you can provide.
I’m not sure what other components may be in question the may be in circuit with the area marked SPEED.
I may have failed to mention the condition.
Speedometer is reading close to double the actual speed at any speed.
Not all the parts would be bad and in need of replacement. I’m not sure which ones may be bad that give a false reading. You’re best option would be to contact a service garage that can diagnose what the issue is with the speedometer.
Steve
I am the service garage.
In most cases you would replace the entire cluster.
In this case I am trying to get this car ready for my granddaughter on the cheap.
I don’t mind replacing the components since from what I can find most are low cost.
I just need to identify them in order to get the right ones for the replacement.
Please help if you can.
Thanks again.