What type of resistors do i require

Hi, i Have a 2010 Hobby prestige caravan which runs on mains electricity 240v has no leisure battery fitted. The issue i have the dometic 240v transformer power supply to 12v does no longer work. There are 2 resistors that have been damaged but I cannot identify what type they are they are on the board . I can’t find a electrical schematic drawing to help the situation.

R9A and R8 resistors.

ò

@ceri.pugh

From the image it looks like the resistors only have 1 color band each?
Would you be able to confirm this? As well as the color(s) each would have?

Hi I can’t at the moment as I’m not with the unit, when I have the opportunity later I will post up hopefully with a reply with the information, but I believe its to badly damaged

I’ve taken some pictures at different angles to see if I can make out the colours of the resistors

It looks like the cours are R9A, Gold ,black red ?

The inner seems to just have 1 red band

@ceri.pugh

For the resistor with the Gold, Black, Red. It is not a normal for it to only be 3 however if it is a 2Ω 5% I found an option below.
Resistor Color Code Calculator - 4 band, 5 band, 6 band | DigiKey Electronics

1712-LR1F2R0CT-ND
LR1F2R0 TE Connectivity Passive Product | Resistors | DigiKey

As for the 1 red band.
I am not sure what that would be other than another 2Ω item.

Thank you Nathan, after your advice a bit of indepeth research ifound out that I require X2 ,

Part No; ROX2SJ22R, see attached photo.

Hope this helps others