Indentifying capacitor with 4 markings

Hi, I would truly be grateful if someone here could help me better indentify this capacitor.

(On an AC to DC Converter) 115-120VAC to 12-14VDC

It has 4 marks on it.
E
472M
1KV
SEC

I Can’t find it on this site im lost in the specs.
I have two on another board that are burnt I would like to replace with identical or equivalent.
Thank you.

Any help will be much appreciated.
Thank you.

Value code “472”
Tolerance code “M”
Voltage = 1kV = 1000V

Reference:
https://www.electronics-tutorials.ws/capacitor/cap_5.html#:~:text=Capacitor%20Tolerance%20Letter%20Codes%20Table

Don’t be fooled by the page title, it also explains the letter code.

So your part is

4700pF = 4.7nF = 0.0047uF
+/-20% (any lower value is OK)
1kV

Here’s the least expensive in stock part:

In case you want to try to match the exact size, here’s the full list of in stock parts:

4700 pF Through Hole Ceramic Capacitors | Electronic Components Distributor DigiKey