I have been testing these units and I have flashed the programmable firmware a single time, but after a power reset they appear to not be reprogrammable. I would like to verify before continuing development.
------Question for VC-02-KIT Please Put your question below------
Hello,
I am checking on this. Will post when I have an answer for you.
This excerpt was taken from the spec sheet:
VC-02-Kit has two methods for firmware upgrade , JTAG debugger program and serial port
program.
JJTAG debugger uses VC series dedicated JTAG debugger, Jlink series debugger are not
supported,The firmware file name being used is:uni_app_release.bin
Serial port program is USB program mode (module requires external TTL to USB
module access to TX1 and RX1), the firmware file name being used must be
uni_app_release_update.bin (cannot rename for āuni_app_release.binā), make sure to use
the ābuild.sh updateā instruction to compile.
If you read bullet point 2 the firmware must have a specific name. Nothing in the spec sheet says the part is OTP, which should be specified, otherwise it should be reprogrammable.
Iāll keep looking.
1 Like
Here is the response from the supplier ā this should help them with their inquiry.
You can share this article with the customer.