Hello,
Thanks for providing this detailed guide at https://forum.digikey.com/t/debian-getting-started-with-the-beaglebone-black/12967
I followed all steps to get a minimal debian system with kernel 5.10.47-bone-rt-r44
going. I now have the problem that there is no output after the Starting kernel… output from the bootloader…
I try to boot from SD card, but there is still a image running on the eMMC. Can this be problematic?
Here is the output before nothing happens anymore:
loading /boot/dtbs/5.10.47-bone-rt-r44/am335x-boneblack.dtb ...
93373 bytes read in 53 ms (1.7 MiB/s)
uboot_overlays: add [enable_uboot_overlays=1] to /boot/uEnv.txt to enable...
debug: [console=ttyO0,115200n8 root=/dev/mmcblk0p1 ro rootfstype=ext4 rootwait] ...
debug: [bootz 0x82000000 - 0x88000000] ...
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe6000, end 8ffffcbc ... OK
Starting kernel ...
Kind Regards
Robin