I purchased Xilinx Kria KV260 Vision AI Starter Kit (Part #: 410-377).
Invoice Date: [23-01-2026]
The board is not working:
**Errors:**
- SD card slot: “Card did not respond to voltage select! : -110”
- USB controller: “probe failed, error -110”
- Ethernet PHY: “PHY reset timed out”
- PS-GTR PHY: “PLL lock timeout, Failed to power on: -110”
**Tested:**
- Multiple SD cards (SanDisk Ultra 32GB, 16GB)
- Different card readers and PCs
- Correct OS (Ubuntu 22.04 ARM64 for Kria)
- Jumpers J18/J21 verified OPEN for SD boot
- Power supply: 12V 5A (60W)
**Board info:**
- Model: KRIA KV260-G
Please check the attached log file and let us know.
logs.txt (2.3 KB)
Hello,
Thank you for posting on our forum.
Please contact Techs@digikey.com
We will need to start the defective process and try to contact the manufacture to help trouble shoot the board.
Please mention case number (Tech Reference Number T4898806)
Subject: Tech Reference Number T4898806
The tech team is not responding. I am attaching the log (error) file for your reference. Manufacturer, , please trouble shoot the error and find out a solution on priority. Please check.
T4898806
logs.txt (2.3 KB)
I had posted my error on AMD. Still, there is no response from them.
Thank you for contacting DigiKey Technical support.
I am sorry to inform you we have no way to expedite your case.
Please give the manufacture more time to answer your question.
I had raised this issue on Feb 6th. Still now, my issue is not yet resolved. If you cannot sort out the issue, replace the product or refund my amount. My project is getting delayed because of the Faulty product. I suggest you to initiate the replacement process. I had already paid Customs duty in my country. It is a waste of time and resources. Your contact number is also not working i.e 8000404249.
We have to go through the full process to get you the return.
I contacted the manufacture, they recommended you post on their forum.
We have no way to expedite your case.
Nathan, we are waiting for a response from your end. I had been delivered a product which has manufacturing defect. Still, no solutions from your end. May I know, Indian office details, so that I can contact them directly. I am losing a valuable resource i.e “TIME”.
Regards,
Sitaram
India
Nathan, this is request on AMD for a solution. No one is responding from AMD.
I have reached out to AMD to request they follow up with you on their Support Forum. We will continue to seek support from them going forward on this issue.
I’m continuing to seek support from AMD on this.