I need to replace this E-Stop button, but I can’t seem to narrow it down to what the part number should be for it. Added photos of the “whole” thing.
Hello JRacek,
Welcome to the DigiKey TechForum! What you have is considered a Configurable Switch, in which the difference pieces can be swapped out for different functions.
The bottom picture you provided is of the Switch Contact Block, and in this case it is a Cutler-Hammer (Division of Eaton) E22B1. It is rated for 10A and 600V, and is a normally closed SPST switch. Unfortunately, we do not carry that specific model, but we do have some that carry the same electrical specifications. You can find those by clicking below:
The components in the first two pictures you provided are the Configurable Switch Bodies. Typically, you will want to choose the contact block first, and then use the switch body that is within the series. Most datasheets will provide the compatible parts within the series and outline what you will need.
Regards,
Klint
Klint, thanks for the reply. I am mainly looking for the push button as this one is broken. The Cutler is what is will be attaching to. So with that, would you be able to narrow down what the push button itself would be part number wise?