Hi all I am looking for a cable with 5 Position M8 Female Connector with UL 105C and No connector on another End I am looking for cable with diameter less than 4.5mm as we will use only two positions out of 5 positions
Could you help me narrow down the selection by answering a few questions? Is the housing female or are the pins inside female? There are combinations where the housing is one gender but the contacts are the other. The next issue is that I cannot search by UL 105C or cable diameter in this particular category of parts. Do you know what length of cable you need? Any extra information that you have will help us narrow things down. I have this list of parts otherwise, click here.
Hi Kaleb Kohlhase, yes, the Housing and Pins must be female and
Length of the cable 1m is enough I am looking for any smaller diameter ones if available.Thanks
Thank you for the information. I was able to narrow the selection down to six parts. Review these options for your application, click here. Check each datasheet and see if there are drawings to learn more about dimensions.
Link is not working it just redirects to complete cable profiles thanks
Sorry about that, I fixed the link above.
Thanks for those suggestions. Is this also a good fit 10-05350
I think that may be a decent selection. Keep in mind this has a specific keying position called “B” in the “Orientation” specification. If your mating connector does not have the same orientation, it won’t work properly. I usually assume the normal “Keying” or “A” type for most applications.