MIKROE-5925, the pin VCM outputs 0V

------Question for MIKROE-5925 Please Put your question below------

MIKROE-5925: The VCM pin should output 2.35V, but it measures 0V relative to GND. The 3.3V mode is selected, and 3.3V and GND are connected.

Hello,

Checking on this one. Will let you know when I have the answer.

The schematic for the board would seem to indicate that the featured device is powered from the 5V supply. The Vcc selection determines the supply reference for the digital interface, but not which supply the SENM3Dx device is powered from.

Thanks for your suggestion. It worked.