Mini-DIN-6 6 pin to 4 pin

Hello I am currently try to to connect this 6 pin female connector to a Capture card (Amazon.ca) which contains 4 pins. Is there a cable that does this ?

@achertov

I am not seeing that we currently list an option that would do that conversion.

If you are able to find enough information to know the connections each side has you can build your own cable to do the conversion.
The below link shows the 4 and 6 mini-din connectors we do list.

Can i use this to connect to my 6 pin female ? (https://www.digikey.ca/en/products/detail/eaton-tripp-lite/P222-006/1533428?gclsrc=aw.ds&&utm_adgroup=&utm_source=google&utm_medium=cpc&utm_campaign=PMax%20Shopping_Product_New%20Customer%20Acquisition&utm_term=&productid=1533428&utm_content=&utm_id=go_cmp-19909744982_adg-_ad-__dev-c_ext-_prd-1533428_sig-CjwKCAjw-qi_BhBxEiwAkxvbkD6kngRbOuuIG3qtUHIgAIlG3IDPRV_eFd7lPRQA8QfJ0sBxBZO3hxoCnDsQAvD_BwE&gad_source=1&gclid=CjwKCAjw-qi_BhBxEiwAkxvbkD6kngRbOuuIG3qtUHIgAIlG3IDPRV_eFd7lPRQA8QfJ0sBxBZO3hxoCnDsQAvD_BwE&gclsrc=aw.ds)

That cable is for PS/2 style. The key is a little different..

Your video device (Capture) uses S-Video: (Mini-DIN-4) Mini-DIN connector - Wikipedia

Regards,

Is there another cable that can be used ?

What device is exporting video (source) over your (Mini-DIN-6) cable? wonder if it’s a custom cable?

Regards,

Looks like they also chain power over the 6-pin..

S-video is 4 pins, GND Y, GND C, Y and C… S-Video - Wikipedia

You’ll need to check the pins on your Mini-DIN-6, to see if you can grab those 4..

A big warning on this connector:
Again, there is no standardization between manufacturers as to which pin does what, and there are two known variants of the connector in use.

Regards,

achertov,

Click Here for some 6 pin Male connectors that may mate to your female connector.
Please check the datasheets to verify compatibility to your application.
If you want a cable, with one end with the 6pos Male connector, Click Here for those options.

Mini-DIN-6 and Mini-DIN-4 have a different key.

https://en.wikipedia.org/wiki/Mini-DIN_connector:

Regards,