Dear sir,i need a setup to collect data from sensors(temperature, BP, Heartbeat etc) placed on body and amplify them and transfer to transmitting antenna and at receiving side a receiving antenna to collect that data and should display on system
Thank you for your inquiry and welcome to the community.
What frequency of communication will you be needing?
Antennas do not typically do well in close proximity to water which a human is over 50% water.
One of the better antennas for use in proximity to human bodies is the Splatch and microSplatch antennas from TE Connectivity Linx
Click here for TE Connectivy Linx Splatch and microSplatch antennas in sub-1Ghz frequencies