This is the connector to the laser on my laser cutter cable. It’s 2mm pitch. There’s a tiny “ZJT” embossed above the first position.
I need to build a new cable and I’ve been looking and looking for what it is, but no luck. If anyone knows, I’d really appreciate it. Thanks!
@TrickyWidget
I am sorry to say that I too may able to ID that connector.
A little different, please review: 2057-2CH-H-08-ND
TrickyWidge,
I have been looking into this as well. These types of connectors can be difficult as there are many products with only small variants. I was not able to find anything that was a dead ringer for the connector and header in the images but I did find something that looked close. really close. I cannot vouch for the pitch as that was not provided. I would also take some measurements of the product you have and compare it with the data sheet to be sure it will work. If it does work, please come back to this post and let us know to help the next person.

| MFR PART # |
353630860 |
| DIGI-KEY PART # |
WM18937-ND |
| MANUFACTURER |
Molex |
| DESCRIPTION |
Connector Header Through Hole, Right Angle 8 position 0.079" (2.00mm) |
| DATASHEET |
Click Here |
and

| MFR PART # |
355070800 |
| DIGI-KEY PART # |
WM5987-ND |
| MANUFACTURER |
Molex |
| DESCRIPTION |
8 Rectangular Connectors - Housings Receptacle Natural 0.079" (2.00mm) |
| DATASHEET |
Click Here |
I do hope this helps!
Those are both close, but I don’t think they would work. They both have guides protruding on either side of the latch that extend all the way down. Since the socket doesn’t have slots to accommodate them, I believe those guides would collide with the front edge of the socket before it could seat.
But thank you both @Ryan_2724 and @AaronRollens for the suggestions!
1 Like