Need help identifying diode

Hello Coreyhauer and welcome to the DigiKey TechForum.

Unfortunately, I was not able to identify this based just on the marking.
Are you able to provide more information about the board with this Diode? Model number or device name?

Yes, it’s in a Mikrotik CCR2216 router. We accidentally blew it up by applying a 24vdc power supply even though it needs 12vdc.

Fair chance it’s a Bencent BV-SMDJ13A.

That would be a fairly generic unidirectional 13V TVS diode for which SMDJ13ACT-ND would be one of many available comparable equivalents. A very reasonable choice for input protection of a 12V supply input, and very much something that would blow promptly if a 24v supply were connected.

Perhaps worth a try to potentially salvage an expensive piece of gear, but there’s a very real chance that additional damage was done that is less visible.