Need help identifying US supplier for a connector used in TDK ultrasonic

Hi,

I bought a TDK USSM ultrasonic sensor module from mouser recently but I’m having trouble finding the right connector for it. According to the datasheet (which I have embedded an image of below) the connector is from SWB and has the part number: 1002WVS-03E-LPSW. I tried to google search the part number but only found the datasheet for the connector itself and no US supplier. If anyone knows if this is available on digikey or elsewhere please let me know! Thanks!

Screenshot from 2023-12-04 16-33-43

Welcome to the Technical Forum. I am not finding any US suppliers either. The only thing I can think of is to try to mate it up to another 3 position 1.0mm receptacle. You can look at these options to see if you can make something work: https://www.digikey.com/short/bt478jc3

Other people do watch this forum also. Maybe someone might offer a better suggestion.

Hi @bcarbo6 ,
The mating housing is 1002H-03E, which is dimensionally almost identical to JST’s SH connector. You could try the SH, if your application is not critical.

There is also other maker (XKB) for the connector.

Could not find any U.S. distributor either.
Cheers, heke

1 Like