New SiTime Custom Part Request

Sorry for the wait. Please check the website tomorrow.

Dear DigiKey,

We need the SIT8021AI-J4-XXS-16.000000E (3.3V, 16Mhz) which is now on long lead times, can you program these from blank parts instead for a smaller quantity (like 100)?

P.S. Now I see that this part was already mentioned, is there anything else you can suggest for these? Almost all 3.3V versions seem to be affected by the shortages.

Best regards

The SiTime parts are working great!

Can you please add SiT2001BC-S3-33N-53.693182 ?

Best Regards,

Hello cwilkson,

I have sent a request to have the part added. The part should be on the website in the next 48 hours. Please check back then.

Thanks!

Hello mbakula,

We currently are unable to program SIT8021AI-J4-XXS-16.000000, and we are hoping to have the availability to program these parts by the end of September.

Also, the closest option we have available is SIT8021AI-J4-18S-16.000000 and its 1.8V instead of 3.3v.

Thanks,

Hello,
We would like to have PN: SIT8920BM-83-33E configured for 9.383 MHz.
SiT8920BM-83-33E-9.383000

Thanks,
Tim

Hello @timcam,

The request has been put in. The part number should be available on the website in the next 48 hours.

Thank you,
Jeff

Dear Digikey,

Could I please get the part ‎SiT2001BC-S1-33N-49.152000 added to your list?

Kind regards.

Thanks for the part addition. I have sent a request to have the part added to the system. Please check the website in the next 48 hours to see the addition.

Thank you,

Jeff

Thanks @Jeff_2258! I can now see the part number online, but I am unable to add it to my cart as it is currently only active, not available. Do I just need to wait a little bit longer? Thanks.

Please wait a little longer. I will see if we can have the price added soon.

Thanks!

Thanks @Jeff_2258. Why is the price $7.49 each and not $1.85 like the SIT2001BC-S1-33N-21.168000 is? That price difference seems excessive? It’s the same part with a different clock frequency. Regards.

Could I ask; who gave you that pricing? What currency are you using?

@Jeff_2258 - The DigiKey Australia website, in AUD. For both components.

And the website just mysteriously changed price… thanks!

The Price would be $1.85 AUD. The website should be updated with the price breaks soon.

Thanks,

Dear DigiKey,
I’d like to order SiTime part number SIT5186AI-FA-30VT-26.000000.
Can you please add it to your website?

Welcome to the community!

We might not be set up to program the 5186. I’m checking into this for you.

Thanks!
Jeff,

We are not set up to program this part SIT5186AI-FA-30VT-26.000000. We will have to do a non-catalog request for the item, where we check with the manufacturer for their manufacturing minimums, price and lead times. It typically takes 3-5 business days to get the quote back.

Send me a private message if you are interested in the quote.

Thanks!

Dear Jeff,

Can you provide any updates on the SIT8021AI-J4-XXS-16.000000 part, can you program these by now?

It needs to be able to work on 3.3V and for the other part this is not clear, indeed the datasheet only states one maximum voltage rating (3.6V). Does it mean that the 1.8V parts can also work with 3.3V, maybe with reduced performance (i.e. higher current consumption), can you advise on this?

Best regards,

I’m checking on the update for SIT8021AI-J4-XXS-16.000000.

Thanks!