This post is for informational purposes only. Please review the specifications and manufacturer datasheet before purchasing any parts for use in your project.
NF-PS-EZJ192L24 is an LED driver made by Nova Flex. We don’t carry this product line but if you have trouble sourcing it part number 1866-ELG-240-24DA-3Y-ND from Mean Well may work as an alternative. It meets or exceeds the power specifications, though it is definitely overkill at 10A max the current can be adjusted down. This is not a direct cross-reference to the original, but this could be useful if you need to upgrade the max power that you’re getting out of a 2-output driver.
See below for more details on this alternative option.
| MFR PART # | ELG-240-24DA-3Y |
|---|---|
| DIGIKEY PART # | 1866-ELG-240-24DA-3Y-ND |
| MANUFACTURER | MEAN WELL USA Inc. |
| DESCRIPTION | LED AC/DC DRIVER 240W |
| DATASHEET | Click Here |