Does it matter how I wire up my outputs for the F3SG-SR?
- No, the F2SG-SR can auto-sense the NPN/PNP outputs.
Do I need to add a safety mat to a machine that had blind spots for pre-reset with this light curtain?
- No. The F3SG-SR has built-in pre-reset capability for added protection to machines with blind spots.
Can you cascade F3SG-SR light curtains?
- Yes, you can cascade up to 255 beams, which is based on the number of light curtains you can determine the length that you can do this.
How many F3SG-SR can you connect via optical synchronization (no sync wire lines)?
- F3SG-SR can connect up to 2 sets using optical synchronization (no sync wire lines).

For further details on the F3SG-SR light curtains please refer to the manufacturer datasheet below.
Applicable Part Numbers
F3SG-4SRA0280-25-F F3SG-4SRA0440-25-F F3SG-4SRA0400-14 F3SG-4SRA0600-25-F F3SG-4SRA0560-14 F3SG-4SRA0760-25-F F3SG-4SRA0920-25-F F3SG-4SRA0720-14-F F3SG-4SRA0880-14-F F3SG-4SRA1200-25 F3SG-4SRA1200-14 F3SG-4SRA1600-25 F3SG-4SRA1760-25 F3SG-4SRB0280-85 F3SG-4SRB0240-45 F3SG-4SRA0280-85 F3SG-4SRA0240-45 F3SG-4SRB0160-25 F3SG-4SRB0440-85 F3SG-4SRB0200-25-F F3SG-4SRB0400-45 F3SG-4SRB0240-25 F3SG-4SRB0280-25-F F3SG-4SRB0160-14 F3SG-4SRB0320-25 F3SG-4SRA0160-25 F3SG-4SRB0200-14-F F3SG-4SRB0360-25-F F3SG-4SRA0200-25-F F3SG-4SRA0440-85 F3SG-4SRB0240-14 F3SG-4SRA0240-25 F3SG-4SRA0400-45 F3SG-4SRB0400-25 F3SG-4SRB0280-14-F F3SG-4SRB0600-85 F3SG-4SRB0560-45 F3SG-4SRA0160-14 F3SG-4SRB0320-14 F3SG-4SRA0320-25 F3SG-4SRB0440-25-F F3SG-4SRA0200-14-F F3SG-4SRA0360-25-F F3SG-4SRA0240-14 F3SG-4SRB0360-14-F F3SG-4SRB0480-25 F3SG-4SRB0760-85 F3SG-4SRA0400-25 F3SG-4SRA0280-14-F F3SG-4SRB0720-45 F3SG-4SRB0520-25-F F3SG-4SRB0400-14 F3SG-4SRA0600-85 F3SG-4SRA0320-14 F3SG-4SRA0560-45 F3SG-4SRB0560-25 F3SG-4SRB0920-85 F3SG-4SRB0880-45 F3SG-4SRB0440-14-F F3SG-4SRA0360-14-F F3SG-4SRA0480-25 F3SG-4SRB0600-25-F F3SG-4SRA0760-85 F3SG-4SRB0480-14 F3SG-4SRA0720-45 F3SG-4SRB0640-25 F3SG-4SRA0520-25-F F3SG-4SRB0680-25-F F3SG-4SRB0520-14-F F3SG-4SRA0560-25 F3SG-4SRA0440-14-F F3SG-4SRB0720-25 F3SG-4SRA0920-85 F3SG-4SRA0880-45 F3SG-4SRB0560-14 F3SG-4SRB0760-25-F F3SG-4SRB1200-45 F3SG-4SRA0480-14 F3SG-4SRB0600-14-F F3SG-4SRA0640-25 F3SG-4SRB0800-25 F3SG-4SRA0680-25-F F3SG-4SRB0640-14 F3SG-4SRA0520-14-F F3SG-4SRB0840-25-F F3SG-4SRA0720-25 F3SG-4SRB0880-25 F3SG-4SRB0680-14-F F3SG-4SRB0920-25-F F3SG-4SRB0720-14-F F3SG-4SRB1520-45 F3SG-4SRA1200-45 F3SG-4SRA0600-14-F F3SG-4SRB0960-25 F3SG-4SRB0760-14-F F3SG-4SRA0800-25 F3SG-4SRB0800-14 F3SG-4SRA0640-14 F3SG-4SRB1000-25-F F3SG-4SRA0840-25-F F3SG-4SRB0840-14-F F3SG-4SRA0880-25 F3SG-4SRA0680-14-F F3SG-4SRB1040-25 F3SG-4SRB0880-14-F F3SG-4SRA0960-25 F3SG-4SRA0760-14-F F3SG-4SRA1520-45 F3SG-4SRB0920-14-F F3SG-4SRB1120-25 F3SG-4SRA0800-14 F3SG-4SRA1000-25-F F3SG-4SRB1200-25 F3SG-4SRA0840-14-F F3SG-4SRB0960-14-F F3SG-4SRA1040-25 F3SG-4SRB1280-25 F3SG-4SRB1000-14 F3SG-4SRA0920-14-F F3SG-4SRA1120-25 F3SG-4SRB1360-25 F3SG-4SRB1440-25 F3SG-4SRA0960-14-F F3SG-4SRB1200-14 F3SG-4SRA1280-25 F3SG-4SRB1520-25 F3SG-4SRA1000-14 F3SG-4SRB1600-25 F3SG-4SRA1360-25 F3SG-4SRB1680-25 F3SG-4SRA1440-25 F3SG-4SRB1400-14 F3SG-4SRB1760-25 F3SG-4SRA1520-25 F3SG-4SRB1840-25 F3SG-4SRB1920-25 F3SG-4SRA1680-25 F3SG-4SRB1600-14 F3SG-4SRB2080-25 F3SG-4SRA1400-14 F3SG-4SRA1840-25 F3SG-4SRB2280-25 F3SG-4SRB1800-14 F3SG-4SRA1920-25 F3SG-4SRA1600-14 F3SG-4SRA2080-25 F3SG-4SRB2480-25 F3SG-4SRB2000-14 F3SG-4SRA2280-25 F3SG-4SRA1800-14 F3SG-4SRA2480-25 F3SG-4SRA2000-14